<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: S32 DS v2.2 processor expert error messages</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047617#M6195</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is new project with adding lpspi component from processor expert.  I also notice that when I open the project with lpspi component, these error message will pop up as well.&lt;/P&gt;&lt;P&gt;This is not happen for this v2.2 DS, it is also happen on R2018.R1 DS as well.  However, there was no error during compilation of the code and code working as I expected.&lt;/P&gt;&lt;P&gt;I am not too concern about this, but just want to know why.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cuong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 14:10:43 GMT</pubDate>
    <dc:creator>cuongtran</dc:creator>
    <dc:date>2020-06-04T14:10:43Z</dc:date>
    <item>
      <title>S32 DS v2.2 processor expert error messages</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047615#M6193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when I start opening a project in S32 DS V2.2, the following messages showed up.&amp;nbsp; Does any one know why??&lt;/P&gt;&lt;P&gt;and how can&amp;nbsp; I get rid of these error messages?.&amp;nbsp; Thanks.&lt;/P&gt;&lt;P&gt;&lt;IMG /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2020 18:58:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047615#M6193</guid>
      <dc:creator>cuongtran</dc:creator>
      <dc:date>2020-06-02T18:58:14Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS v2.2 processor expert error messages</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047616#M6194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's your project? It is an example or some old project which you like to migrate into new S32DS?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 13:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047616#M6194</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2020-06-04T13:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32 DS v2.2 processor expert error messages</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047617#M6195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is new project with adding lpspi component from processor expert.  I also notice that when I open the project with lpspi component, these error message will pop up as well.&lt;/P&gt;&lt;P&gt;This is not happen for this v2.2 DS, it is also happen on R2018.R1 DS as well.  However, there was no error during compilation of the code and code working as I expected.&lt;/P&gt;&lt;P&gt;I am not too concern about this, but just want to know why.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cuong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 14:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-DS-v2-2-processor-expert-error-messages/m-p/1047617#M6195</guid>
      <dc:creator>cuongtran</dc:creator>
      <dc:date>2020-06-04T14:10:43Z</dc:date>
    </item>
  </channel>
</rss>