<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: MPC5744P can not debug with PE Multilink universal debugger</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044261#M6151</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You might censor the board if you program a DCF record into DFLASH as indicated by Lukas.&lt;/P&gt;&lt;P&gt;Anyway if you can connect and debug one board only, it may indicate probably a hw issue with the other board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check:&lt;/P&gt;&lt;P&gt;* Pemicro probe LEDs (blue, yellow) are ON when the board is powered up?&lt;/P&gt;&lt;P&gt;* is there a reasonable power consumption when you power up the board. Please check the power supply voltages for MCU&lt;/P&gt;&lt;P&gt;* Boot mode signals (FAB/ ABS) set to boot from internal flash?&lt;/P&gt;&lt;P&gt;* can check if crystal clock is oscillating and&lt;/P&gt;&lt;P&gt;* state of the RESET line (as suggested by Lucas)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps...&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Aug 2020 13:00:43 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2020-08-24T13:00:43Z</dc:date>
    <item>
      <title>MPC5744P can not debug with PE Multilink universal debugger</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044259#M6149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP:&lt;/P&gt;&lt;P&gt;I have two boards of we own designed, In the beginning, two boards can debug with&amp;nbsp;PE Multilink universal debugger, I dont't know what happened, Now one board can not dubug with&amp;nbsp;PE Multilink universal debugger，the fault message tips in the following figure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115244i1CF2ECF5A7E49D63/image-size/large?v=v2&amp;amp;px=999" title="微信截图_20200819140208.png" alt="微信截图_20200819140208.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 06:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044259#M6149</guid>
      <dc:creator>1067929469</dc:creator>
      <dc:date>2020-08-19T06:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P can not debug with PE Multilink universal debugger</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044260#M6150</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;did you check the reset line? Is it deasserted after power on?&lt;/P&gt;&lt;P&gt;Did you touch censorship information or DCF records before that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 05:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044260#M6150</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-08-20T05:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5744P can not debug with PE Multilink universal debugger</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044261#M6151</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You might censor the board if you program a DCF record into DFLASH as indicated by Lukas.&lt;/P&gt;&lt;P&gt;Anyway if you can connect and debug one board only, it may indicate probably a hw issue with the other board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check:&lt;/P&gt;&lt;P&gt;* Pemicro probe LEDs (blue, yellow) are ON when the board is powered up?&lt;/P&gt;&lt;P&gt;* is there a reasonable power consumption when you power up the board. Please check the power supply voltages for MCU&lt;/P&gt;&lt;P&gt;* Boot mode signals (FAB/ ABS) set to boot from internal flash?&lt;/P&gt;&lt;P&gt;* can check if crystal clock is oscillating and&lt;/P&gt;&lt;P&gt;* state of the RESET line (as suggested by Lucas)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;hope it helps...&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 13:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5744P-can-not-debug-with-PE-Multilink-universal-debugger/m-p/1044261#M6151</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2020-08-24T13:00:43Z</dc:date>
    </item>
  </channel>
</rss>