<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Problem Updating Duty Cycle</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037215#M6105</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;channel 0,I commented this line because not using it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Dec 2019 19:08:40 GMT</pubDate>
    <dc:creator>huda_abdalla</dc:creator>
    <dc:date>2019-12-12T19:08:40Z</dc:date>
    <item>
      <title>Problem Updating Duty Cycle</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037213#M6103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #222222; background-color: #ffffff; font-size: 14px;"&gt;Using&amp;nbsp;S32K144(WITHOUT SDK) I would like to update the value of the pwm[FTM0_CH0] duty cycle from the output of ADC0&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;...I'm able to read the value of the ADC using software trigger and confirm its operation using Real Time Expressions. However, I'm not able to update the value of the duty cycle with the value of the adc using the command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* EXAMPLE CODE&lt;BR /&gt;*&lt;BR /&gt;* This file is provided as an example on how to use Micrium products.&lt;BR /&gt;*&lt;BR /&gt;* Please feel free to use any application code labeled as 'EXAMPLE CODE' in&lt;BR /&gt;* your application products. Example code may be used as is, in whole or in&lt;BR /&gt;* part, or may be used as a reference only. This file can be modified as&lt;BR /&gt;* required to meet the end-product requirements.&lt;BR /&gt;*&lt;BR /&gt;* Please help us continue to provide the Embedded community with the finest&lt;BR /&gt;* software available. Your honesty is greatly appreciated.&lt;BR /&gt;*&lt;BR /&gt;* You can find our product's user manual, API reference, release notes and&lt;BR /&gt;* more information at &lt;A href="https://doc.micrium.com" target="test_blank"&gt;https://doc.micrium.com&lt;/A&gt;.&lt;BR /&gt;* You can contact us at &lt;A href="https://community.nxp.com/www.micrium.com" target="test_blank"&gt;www.micrium.com&lt;/A&gt;.&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*&lt;BR /&gt;* uC/OS-III&lt;BR /&gt;* EXAMPLE CODE&lt;BR /&gt;*&lt;BR /&gt;* Filename : main.c&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* INCLUDE FILES&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;#include &amp;lt;cpu.h&amp;gt;&lt;BR /&gt;#include &amp;lt;lib_mem.h&amp;gt;&lt;BR /&gt;#include &amp;lt;os.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_os.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_clk.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_int.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_led.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_adc.h&amp;gt;&lt;/P&gt;&lt;P&gt;#include &amp;lt;bsp_timer.h&amp;gt;&lt;BR /&gt;#include &amp;lt;bsp_switch.h&amp;gt;&lt;BR /&gt;#include "os_app_hooks.h"&lt;BR /&gt;#include "../app_cfg.h"&lt;BR /&gt;#include &amp;lt;lib_def.h&amp;gt;&lt;BR /&gt;#include "bsp_adc.h"&lt;BR /&gt;#include "S32K144.h"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* LOCAL DEFINES&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* LOCAL GLOBAL VARIABLES&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;static OS_TCB StartupTaskTCB;&lt;BR /&gt;static CPU_STK StartupTaskStk[APP_CFG_STARTUP_TASK_STK_SIZE];&lt;BR /&gt;static CPU_STK refresh_pwm_stk[APP_CFG_STARTUP_TASK_STK_SIZE];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;static OS_TCB refresh_pwm_tcb;&lt;BR /&gt;extern volatile CPU_INT16U ADC0_adc_chx;&lt;BR /&gt;volatile CPU_INT16U adcResultInMv_pot;&lt;BR /&gt;//volatile OS_SEM ADC0sem;&lt;BR /&gt; OS_SEM ADC0sem;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* FUNCTION PROTOTYPES&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;static void StartupTask (void *p_arg);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* main()&lt;BR /&gt;*&lt;BR /&gt;* Description : This is the standard entry point for C code. It is assumed that your code will call&lt;BR /&gt;* main() once you have performed all necessary initialization.&lt;BR /&gt;*&lt;BR /&gt;* Arguments : none&lt;BR /&gt;*&lt;BR /&gt;* Returns : none&lt;BR /&gt;*&lt;BR /&gt;* Notes : none&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;int main (void)&lt;BR /&gt;{&lt;BR /&gt; OS_ERR os_err;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; BSP_ClkInit(); /* Initialize the main clock. */&lt;BR /&gt; BSP_IntInit();&lt;BR /&gt; BSP_OS_TickInit(); /* Initialize kernel tick timer */&lt;/P&gt;&lt;P&gt;Mem_Init(); /* Initialize Memory Managment Module */&lt;BR /&gt; CPU_IntDis(); /* Disable all Interrupts. */&lt;BR /&gt; CPU_Init(); /* Initialize the uC/CPU services */&lt;/P&gt;&lt;P&gt;OSInit(&amp;amp;os_err); /* Initialize uC/OS-III */&lt;BR /&gt; if (os_err != OS_ERR_NONE) {&lt;BR /&gt; while (1);&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;App_OS_SetAllHooks(); /* Set all applications hooks */&lt;/P&gt;&lt;P&gt;OSTaskCreate(&amp;amp;StartupTaskTCB, /* Create the startup task */&lt;BR /&gt; "Startup Task",&lt;BR /&gt; StartupTask,&lt;BR /&gt; 0u,&lt;BR /&gt; APP_CFG_STARTUP_TASK_PRIO,&lt;BR /&gt; &amp;amp;StartupTaskStk[0u],&lt;BR /&gt; StartupTaskStk[APP_CFG_STARTUP_TASK_STK_SIZE / 10u],&lt;BR /&gt; APP_CFG_STARTUP_TASK_STK_SIZE,&lt;BR /&gt; 0u,&lt;BR /&gt; 0u,&lt;BR /&gt; 0u,&lt;BR /&gt; (OS_OPT_TASK_STK_CHK | OS_OPT_TASK_STK_CLR),&lt;BR /&gt; &amp;amp;os_err);&lt;BR /&gt; if (os_err != OS_ERR_NONE) {&lt;BR /&gt; while (1);&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;OSStart(&amp;amp;os_err); /* Start multitasking (i.e. give control to uC/OS-III) */&lt;/P&gt;&lt;P&gt;while (DEF_ON) { /* Should Never Get Here. */&lt;BR /&gt; ;&lt;BR /&gt; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;/*&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;* STARTUP TASK&lt;BR /&gt;*&lt;BR /&gt;* Description : This is an example of a startup task. As mentioned in the book's text, you MUST&lt;BR /&gt;* initialize the ticker only once multitasking has started.&lt;BR /&gt;*&lt;BR /&gt;* Arguments : p_arg is the argument passed to 'StartupTask()' by 'OSTaskCreate()'.&lt;BR /&gt;*&lt;BR /&gt;* Returns : none&lt;BR /&gt;*&lt;BR /&gt;* Notes : 1) The first line of code is used to prevent a compiler warning because 'p_arg' is not&lt;BR /&gt;* used. The compiler should not generate any code for this statement.&lt;BR /&gt;*********************************************************************************************************&lt;BR /&gt;*/&lt;/P&gt;&lt;P&gt;static void StartupTask (void *p_arg)&lt;BR /&gt;{&lt;BR /&gt; OS_ERR os_err;&lt;BR /&gt; /* CPU_INT08U rgb_led_color;*/&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; (void)p_arg;&lt;/P&gt;&lt;P&gt;OS_TRACE_INIT(); /* Initialize Trace recorder */&lt;/P&gt;&lt;P&gt;BSP_OS_TickEnable(); /* Enable the tick timer and interrupt */&lt;/P&gt;&lt;P&gt;#if OS_CFG_STAT_TASK_EN &amp;gt; 0u&lt;BR /&gt; OSStatTaskCPUUsageInit(&amp;amp;os_err); /* Compute CPU capacity with no task running */&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;#ifdef CPU_CFG_INT_DIS_MEAS_EN&lt;BR /&gt; CPU_IntDisMeasMaxCurReset();&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BSP_ADC0_init_polling();&lt;BR /&gt; BSP_FTM0_PWM_Init ();&lt;/P&gt;&lt;P&gt;while (DEF_TRUE) /* Task body, always written as an infinite loop */&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;// FTM0-&amp;gt;CONTROLS[2].CnV= adcResultInMv_pot; /*red*/&lt;BR /&gt; BSP_ADC0_convertAdcChan_polling(12);&lt;BR /&gt; while(BSP_ADC0_adc_complete()==0){}&lt;BR /&gt; adcResultInMv_pot = BSP_ADC0_read_adc_chx();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;}###&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 18:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037213#M6103</guid>
      <dc:creator>huda_abdalla</dc:creator>
      <dc:date>2019-12-11T18:23:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Updating Duty Cycle</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037214#M6104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Would you please confirm which channel you want to update.(Channel 0 or Channel 2?)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96553i8C5E4765CB2832EA/image-size/large?v=v2&amp;amp;px=999" title="error.png" alt="error.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Best Regards,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Robin&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 01:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037214#M6104</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-12-12T01:24:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Updating Duty Cycle</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037215#M6105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;channel 0,I commented this line because not using it&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2019 19:08:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037215#M6105</guid>
      <dc:creator>huda_abdalla</dc:creator>
      <dc:date>2019-12-12T19:08:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problem Updating Duty Cycle</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037216#M6106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;But I didn't found where you change duty of FTM0_CH0.&lt;/P&gt;&lt;P&gt;During debug, does the FTM counter increasing?&lt;/P&gt;&lt;P&gt;Please&amp;nbsp;check the value of FTM0_C0SC\&amp;nbsp;PORT_PCRn&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Best Regards,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;Robin&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 00:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Problem-Updating-Duty-Cycle/m-p/1037216#M6106</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2019-12-17T00:43:34Z</dc:date>
    </item>
  </channel>
</rss>