<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 ADC reading Port Init dependency</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/ADC-reading-Port-Init-dependency/m-p/1020956#M5957</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read an ADC channel reading from one of my pin (example PTC19).&lt;/P&gt;&lt;P&gt;In order to do this should I do the port initialization of PTC19?. or can I read ADC just configuring ADC module only?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Mar 2020 11:30:20 GMT</pubDate>
    <dc:creator>rijil_kp</dc:creator>
    <dc:date>2020-03-12T11:30:20Z</dc:date>
    <item>
      <title>ADC reading Port Init dependency</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ADC-reading-Port-Init-dependency/m-p/1020956#M5957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to read an ADC channel reading from one of my pin (example PTC19).&lt;/P&gt;&lt;P&gt;In order to do this should I do the port initialization of PTC19?. or can I read ADC just configuring ADC module only?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2020 11:30:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ADC-reading-Port-Init-dependency/m-p/1020956#M5957</guid>
      <dc:creator>rijil_kp</dc:creator>
      <dc:date>2020-03-12T11:30:20Z</dc:date>
    </item>
    <item>
      <title>Re: ADC reading Port Init dependency</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ADC-reading-Port-Init-dependency/m-p/1020957#M5958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rijil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by default, pins with analog function (ADC or CMP) are configured as analog pins. Pins without analog function are disabled (the only exceptions are JTAG pins).&lt;/P&gt;&lt;P&gt;So, it's not necessary to configure the pins if the pins are in default reset state (PORT_PCRn[MUX] = 0).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103176iE584624EC610B8AB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_647.png" alt="pastedImage_647.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 05:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ADC-reading-Port-Init-dependency/m-p/1020957#M5958</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2020-03-13T05:45:01Z</dc:date>
    </item>
  </channel>
</rss>