<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: s32v234 chip spi0 pin setting</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/s32v234-chip-spi0-pin-setting/m-p/1007129#M5800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably something went wrong with IO muxing registers setting. Try check actual values of following registers:&lt;/P&gt;&lt;P&gt;SIUL2_MSCR72&amp;nbsp; (SIUL2 offset 0x360);&lt;/P&gt;&lt;P&gt;SIUL2_MSCR73&amp;nbsp; (SIUL2 offset 0x364);&lt;/P&gt;&lt;P&gt;SIUL2_MSCR75&amp;nbsp; (SIUL2 offset 0x36C);&lt;/P&gt;&lt;P&gt;SIUL2_IMCR288&amp;nbsp; (SIUL2 offset 0xEC0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jan 2020 05:54:38 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2020-01-08T05:54:38Z</dc:date>
    <item>
      <title>s32v234 chip spi0 pin setting</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32v234-chip-spi0-pin-setting/m-p/1007128#M5799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;I am using s32v234 chip.&lt;BR /&gt;There is a question about spi0 pin of s32v234 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the figure below, SPI0 can use two pin groups.&lt;/P&gt;&lt;P&gt;I modified the DT to pin SPI0 to port E.&lt;BR /&gt;However, no data is output to Port E.&lt;BR /&gt;If SPI0 is set to Port B, data is output.&lt;/P&gt;&lt;P&gt;What should I do to use SPI0's Pin as Port E?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98624iEFF7DEC4DB8981D9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98625iB6587555B12867CA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DT:&lt;/P&gt;&lt;P&gt;&amp;amp;spi0 {&lt;BR /&gt; #address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt; #size-cells = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;pinctrl-names = "default";&lt;BR /&gt; pinctrl-0 = &amp;lt;&amp;amp;pinctrl_dspi0&amp;gt;;&lt;/P&gt;&lt;P&gt;status = "okay";&lt;/P&gt;&lt;P&gt;spidev0: spidev@0 {&lt;BR /&gt; compatible = "spidev", "nxp,saf5x00";&lt;BR /&gt; spi-max-frequency = &amp;lt;4000000&amp;gt;;&lt;BR /&gt; spi-extended-mode;&lt;BR /&gt; fsl,spi-cs-sck-delay = &amp;lt;500&amp;gt;; // 500ns&lt;BR /&gt; fsl,spi-sck-cs-delay = &amp;lt;500&amp;gt;; // 500ns&lt;BR /&gt; reg = &amp;lt;0&amp;gt;;&lt;BR /&gt; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;pinctrl {&lt;BR /&gt; status = "okay";&lt;/P&gt;&lt;P&gt;s32v234-evb29288 {&lt;BR /&gt; pinctrl_dspi0: dspi0grp {&lt;BR /&gt; fsl,pins = &amp;lt;&lt;BR /&gt; S32V234_PAD_PE9__SPI0_SOUT_OUT&lt;BR /&gt; S32V234_PAD_PE10__SPI0_SIN_OUT&lt;BR /&gt; S32V234_PAD_PE10__SPI0_SIN_IN&lt;BR /&gt; S32V234_PAD_PE8__SPI0_SCK_OUT&lt;BR /&gt; S32V234_PAD_PE11__SPI0_CS0_OUT&lt;BR /&gt; &amp;gt;;&lt;BR /&gt; };&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2019 03:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32v234-chip-spi0-pin-setting/m-p/1007128#M5799</guid>
      <dc:creator>tom3</dc:creator>
      <dc:date>2019-12-23T03:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: s32v234 chip spi0 pin setting</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32v234-chip-spi0-pin-setting/m-p/1007129#M5800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably something went wrong with IO muxing registers setting. Try check actual values of following registers:&lt;/P&gt;&lt;P&gt;SIUL2_MSCR72&amp;nbsp; (SIUL2 offset 0x360);&lt;/P&gt;&lt;P&gt;SIUL2_MSCR73&amp;nbsp; (SIUL2 offset 0x364);&lt;/P&gt;&lt;P&gt;SIUL2_MSCR75&amp;nbsp; (SIUL2 offset 0x36C);&lt;/P&gt;&lt;P&gt;SIUL2_IMCR288&amp;nbsp; (SIUL2 offset 0xEC0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 05:54:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32v234-chip-spi0-pin-setting/m-p/1007129#M5800</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2020-01-08T05:54:38Z</dc:date>
    </item>
  </channel>
</rss>