<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 How to use S32DS debugger 'Program Partition Command'</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-use-S32DS-debugger-Program-Partition-Command/m-p/996557#M5711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use 'advanced' debugger settings to partition S32K144 EVB memory for EEPROM functionality. In S32DS for ARM v2.2. I have mixed results:&lt;/P&gt;&lt;P&gt;- started with default konfig. with FCFG1:DEPART showing 0xC (FlexNVM used as D-Flash)&lt;/P&gt;&lt;P&gt;- next I've tried set 'Enable Partitioning for the device' with 0204 code (all FlexNVM used for EEPROM)&lt;/P&gt;&lt;P&gt;- after clicking Debug - I could still see&amp;nbsp;&lt;SPAN&gt;FCFG1:DEPART showing 0xC (unchanged)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- after a few experiments I've checked both options: 'Emergency Kinetis Device recovery...' and 'Enable Partitioning for the device' (with 0204) - and this worked. I could see&amp;nbsp;FCFG1:DEPART showing 0x4.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- I've experimented with EEPROM functionality - and it has worked as expected&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- then I've checked again 'Emergency Kinetis Device recovery' together with 'Enable Partitioning for the device' with code '020C' to restore FlexNVM as D-Flash. After 'Debug' I could see&amp;nbsp;FCFG1:DEPART showing 0xF which is 'FlexNVM not assigned'. After that I could not change this&amp;nbsp;field any more (no option 020C or 0204 works this time).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can You explain how this function works ? What is the proper sequence of actions to successfully partition memory ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why am I seeing such erratic behaviour ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for help&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Maciek&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Mar 2020 19:30:46 GMT</pubDate>
    <dc:creator>Maciek</dc:creator>
    <dc:date>2020-03-20T19:30:46Z</dc:date>
    <item>
      <title>How to use S32DS debugger 'Program Partition Command'</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-use-S32DS-debugger-Program-Partition-Command/m-p/996557#M5711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to use 'advanced' debugger settings to partition S32K144 EVB memory for EEPROM functionality. In S32DS for ARM v2.2. I have mixed results:&lt;/P&gt;&lt;P&gt;- started with default konfig. with FCFG1:DEPART showing 0xC (FlexNVM used as D-Flash)&lt;/P&gt;&lt;P&gt;- next I've tried set 'Enable Partitioning for the device' with 0204 code (all FlexNVM used for EEPROM)&lt;/P&gt;&lt;P&gt;- after clicking Debug - I could still see&amp;nbsp;&lt;SPAN&gt;FCFG1:DEPART showing 0xC (unchanged)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- after a few experiments I've checked both options: 'Emergency Kinetis Device recovery...' and 'Enable Partitioning for the device' (with 0204) - and this worked. I could see&amp;nbsp;FCFG1:DEPART showing 0x4.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- I've experimented with EEPROM functionality - and it has worked as expected&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;- then I've checked again 'Emergency Kinetis Device recovery' together with 'Enable Partitioning for the device' with code '020C' to restore FlexNVM as D-Flash. After 'Debug' I could see&amp;nbsp;FCFG1:DEPART showing 0xF which is 'FlexNVM not assigned'. After that I could not change this&amp;nbsp;field any more (no option 020C or 0204 works this time).&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can You explain how this function works ? What is the proper sequence of actions to successfully partition memory ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why am I seeing such erratic behaviour ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for help&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Maciek&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 19:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-use-S32DS-debugger-Program-Partition-Command/m-p/996557#M5711</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2020-03-20T19:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to use S32DS debugger 'Program Partition Command'</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-use-S32DS-debugger-Program-Partition-Command/m-p/996558#M5712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Maciek,&lt;/P&gt;&lt;P&gt;This is PE Micro GDB Server Plug-In, please contact PE Micro Support if you have any issues with the plugin.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320151&amp;amp;productTab=1" title="http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320151&amp;amp;productTab=1"&gt;GDB Server Plug-In for Eclipse-based ARM IDEs | PEmicro plug-in for working with freely downloadable GDB Debugger | PEmi…&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;GDB Server Plug-In for Eclipse-based ARM® IDEs&amp;nbsp;Debug Configuration User Guide, v.1.06&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/downloads/download_file.cfm?download_id=459"&gt;www.pemicro.com/downloads/download_file.cfm?download_id=459&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FCFG1:DEPART = 0xC is not&amp;nbsp;the default erased value.&lt;/P&gt;&lt;P&gt;So, I understand that it could not partition the MCU without mass-erasing it first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/104145i42D2BD15302A8476/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_100.png" alt="pastedImage_100.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried launching the FTFC partition command from the application itself?&lt;/P&gt;&lt;P&gt;Just to exclude any potential issues with the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;BR, Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2020 12:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-use-S32DS-debugger-Program-Partition-Command/m-p/996558#M5712</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2020-03-25T12:58:46Z</dc:date>
    </item>
  </channel>
</rss>