<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to setup PFE driver in s32g274a in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976905#M5511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the solution, there are bsp image with the PFE driver included. Beside it, you can use yocto to convert .elf to .bin&lt;/P&gt;&lt;P&gt;only the .bin files will work in linux image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Yihan Cheng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Mar 2020 09:58:20 GMT</pubDate>
    <dc:creator>yihan_cheng</dc:creator>
    <dc:date>2020-03-03T09:58:20Z</dc:date>
    <item>
      <title>How to setup PFE driver in s32g274a</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976904#M5510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded the PFE Firmware file &lt;STRONG&gt;class_s32g.elf&lt;/STRONG&gt;. But I don't know how to setup it.&lt;/P&gt;&lt;P&gt;In the user manuel said:&lt;/P&gt;&lt;P&gt;&lt;EM&gt; The fi rmware binary available on the target either in the  le system or built into the driver depending on which driver is being used.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I copy &lt;STRONG&gt;class_s32g.elf&lt;/STRONG&gt; to the root filesystem from my board in /lib/firmware/, however when i boot the EVB&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PFEng firmware file 'mmc@0:1:pfe-s32g-class.fw' loading failed: -2&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Greeting&lt;/P&gt;&lt;P&gt;Yihan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 08:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976904#M5510</guid>
      <dc:creator>yihan_cheng</dc:creator>
      <dc:date>2020-03-03T08:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup PFE driver in s32g274a</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976905#M5511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the solution, there are bsp image with the PFE driver included. Beside it, you can use yocto to convert .elf to .bin&lt;/P&gt;&lt;P&gt;only the .bin files will work in linux image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Yihan Cheng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 09:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976905#M5511</guid>
      <dc:creator>yihan_cheng</dc:creator>
      <dc:date>2020-03-03T09:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: How to setup PFE driver in s32g274a</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976906#M5512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I do have the same problem.&lt;/P&gt;&lt;P&gt;I have the bsp and yocto recipes for PFE . but from where I will get class_s32g.elf&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 11:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-setup-PFE-driver-in-s32g274a/m-p/976906#M5512</guid>
      <dc:creator>athul_pk</dc:creator>
      <dc:date>2020-07-20T11:00:50Z</dc:date>
    </item>
  </channel>
</rss>