<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Evaluate Sensorless FOC on Dev board # MTRCKTSPS5744P in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Evaluate-Sensorless-FOC-on-Dev-board-MTRCKTSPS5744P/m-p/967665#M5425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the&amp;nbsp;MTRCKTSPS5744P&amp;nbsp;Dev board. It come with a motor and a resolver for position feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Example code provided uses the resolver for the position feedback and I was able to spin the motor with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions is how to evaluate sensorless FOC with this setup (using the same motor and eval board)?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does the source code support sensor less operation? (HW seem to have phase voltage and current feedback)&lt;/LI&gt;&lt;LI&gt;Is it a matter of setup using MCAT to change the default configuration?&lt;/LI&gt;&lt;LI&gt;If so, how to change MCAT? I cannot seem select sensor less option in MCAT?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84692i03C860E6618287B4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jul 2019 14:55:12 GMT</pubDate>
    <dc:creator>rkandiah</dc:creator>
    <dc:date>2019-07-25T14:55:12Z</dc:date>
    <item>
      <title>Evaluate Sensorless FOC on Dev board # MTRCKTSPS5744P</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Evaluate-Sensorless-FOC-on-Dev-board-MTRCKTSPS5744P/m-p/967665#M5425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the&amp;nbsp;MTRCKTSPS5744P&amp;nbsp;Dev board. It come with a motor and a resolver for position feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Example code provided uses the resolver for the position feedback and I was able to spin the motor with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My questions is how to evaluate sensorless FOC with this setup (using the same motor and eval board)?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does the source code support sensor less operation? (HW seem to have phase voltage and current feedback)&lt;/LI&gt;&lt;LI&gt;Is it a matter of setup using MCAT to change the default configuration?&lt;/LI&gt;&lt;LI&gt;If so, how to change MCAT? I cannot seem select sensor less option in MCAT?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84692i03C860E6618287B4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 14:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Evaluate-Sensorless-FOC-on-Dev-board-MTRCKTSPS5744P/m-p/967665#M5425</guid>
      <dc:creator>rkandiah</dc:creator>
      <dc:date>2019-07-25T14:55:12Z</dc:date>
    </item>
  </channel>
</rss>