<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can not program S32K144 EVB in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963204#M5382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear reader(s),&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using S32DS, when I tried to program my EVB, I got this message,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Connection from "127.0.0.1" via 127.0.0.1. Connection from port "59245" to 6224&lt;BR /&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "59246" to 7224&lt;BR /&gt;Telnet server running on 127.0.0.1:51794&lt;BR /&gt;Searching for FreeRTOS Kernel Symbols...&lt;BR /&gt; pxCurrentTCB not found. FreeRTOS analysis not enabled.&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.9.4.201812211851\win32\pegdbserver_console -device=NXP_S32K1xx_S32K144F512M15 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5€&lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.9.4.201812211851\win32\gdi\P&amp;amp;E\supportFiles_ARM\NXP\S32K1xx\freescale_s32k144f512m15_pflash_dflash_eeprom.arp&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;Initialized.&lt;BR /&gt; &lt;BR /&gt;;version 1.04, 11/30/2017, Copyright 2017 P&amp;amp;E Microcomputer Systems, Inc. All rights reserved. &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [s32k144f512m15_x_pflash_dflash_eeprom_rev2]&lt;BR /&gt; &lt;BR /&gt;;device freescale, s32k144f512m15, pflash_dflash_eeprom&lt;BR /&gt; &lt;BR /&gt;;begin_cs device=$00000000, length=$14001000, ram=$20000000&lt;BR /&gt; &lt;BR /&gt;Loading programming algorithm ... &lt;BR /&gt; &lt;BR /&gt;WARNING - Selected .ARP file has been modified. CRC16 = $4977 &lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default} &lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ... &lt;BR /&gt; block 00000000-000013AF ... &lt;BR /&gt; &lt;BR /&gt;Error! CRC Command Timed Out&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;Command is inactive for this .ARP file. &lt;BR /&gt;Error Erasing flash of device &lt;BR /&gt;Error occured during Flash programming. "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the EVB works fine until I wrote to the flash memory 0x1510 using this record,&lt;/P&gt;&lt;P&gt;"S31500001510B841B946BA46BB46BC4606488546064863"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Jun 2019 20:00:12 GMT</pubDate>
    <dc:creator>klau</dc:creator>
    <dc:date>2019-06-07T20:00:12Z</dc:date>
    <item>
      <title>Can not program S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963204#M5382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear reader(s),&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using S32DS, when I tried to program my EVB, I got this message,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Connection from "127.0.0.1" via 127.0.0.1. Connection from port "59245" to 6224&lt;BR /&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "59246" to 7224&lt;BR /&gt;Telnet server running on 127.0.0.1:51794&lt;BR /&gt;Searching for FreeRTOS Kernel Symbols...&lt;BR /&gt; pxCurrentTCB not found. FreeRTOS analysis not enabled.&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.9.4.201812211851\win32\pegdbserver_console -device=NXP_S32K1xx_S32K144F512M15 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5€&lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.9.4.201812211851\win32\gdi\P&amp;amp;E\supportFiles_ARM\NXP\S32K1xx\freescale_s32k144f512m15_pflash_dflash_eeprom.arp&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;Initialized.&lt;BR /&gt; &lt;BR /&gt;;version 1.04, 11/30/2017, Copyright 2017 P&amp;amp;E Microcomputer Systems, Inc. All rights reserved. &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [s32k144f512m15_x_pflash_dflash_eeprom_rev2]&lt;BR /&gt; &lt;BR /&gt;;device freescale, s32k144f512m15, pflash_dflash_eeprom&lt;BR /&gt; &lt;BR /&gt;;begin_cs device=$00000000, length=$14001000, ram=$20000000&lt;BR /&gt; &lt;BR /&gt;Loading programming algorithm ... &lt;BR /&gt; &lt;BR /&gt;WARNING - Selected .ARP file has been modified. CRC16 = $4977 &lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default} &lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ... &lt;BR /&gt; block 00000000-000013AF ... &lt;BR /&gt; &lt;BR /&gt;Error! CRC Command Timed Out&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt;Command is inactive for this .ARP file. &lt;BR /&gt;Error Erasing flash of device &lt;BR /&gt;Error occured during Flash programming. "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the EVB works fine until I wrote to the flash memory 0x1510 using this record,&lt;/P&gt;&lt;P&gt;"S31500001510B841B946BA46BB46BC4606488546064863"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2019 20:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963204#M5382</guid>
      <dc:creator>klau</dc:creator>
      <dc:date>2019-06-07T20:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can not program S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963205#M5383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you able upload RAM target program?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85915iA06D32E60867ABCD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also try Emergency Kinetis device recovery option in debug session confuguration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85916i2C893AFDFBD593FB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 12:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/963205#M5383</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-06-11T12:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can not program S32K144 EVB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/1134231#M6747</link>
      <description>&lt;P&gt;Please share experience if the problem is solved.&lt;/P&gt;&lt;P&gt;I have met the same problem. Works ok in debug_RAM but not in debug_Flash.&lt;/P&gt;&lt;P&gt;Have tried updating openSDA firmware and select the 'Emergency Kinetis...' checkbox. Not working.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2020 12:47:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Can-not-program-S32K144-EVB/m-p/1134231#M6747</guid>
      <dc:creator>smile9999</dc:creator>
      <dc:date>2020-09-02T12:47:02Z</dc:date>
    </item>
  </channel>
</rss>