<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k144 will support CANFD with 5000kbps? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957730#M5284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Jorge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Aug 2019 04:18:56 GMT</pubDate>
    <dc:creator>sreevishakhkp</dc:creator>
    <dc:date>2019-08-16T04:18:56Z</dc:date>
    <item>
      <title>S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957724#M5278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to generate CAN FD message with&amp;nbsp;5000kbps&amp;nbsp; with s32k144. Tried&amp;nbsp; by modifying the sample code which is configured at 500kbps.CAN FD works with 500kbps but not with any other higher bit rates.Please let me know any other changes to be done.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 12:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957724#M5278</guid>
      <dc:creator>sreevishakhkp</dc:creator>
      <dc:date>2019-08-06T12:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957725#M5279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sreevishakh kp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The module by itselft is capable of supporting 5Mbps, for this scenario you would need to use an external oscillator of more than 30MHz and use a setup of the module for the correct time configuration. Our evaluation board uses a osc of 8MHz, so with our EVB it is not possible to achive this baudrate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of this, you would need a transciver capable of that frequency, and also consider that you sampling point will decrease.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 20:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957725#M5279</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-08-08T20:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957726#M5280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Thanks for your replay.&lt;/P&gt;&lt;P&gt;From flexCan component clock configuration its showing at 40MHz external clock only it will configure bit rate to 5000Kbps.Is it possible to use internal clock sources.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86842iA8874311C2B37FA6/image-size/large?v=v2&amp;amp;px=999" title="FlexCAN.png" alt="FlexCAN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 09:37:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957726#M5280</guid>
      <dc:creator>sreevishakhkp</dc:creator>
      <dc:date>2019-08-12T09:37:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957727#M5281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;Sreevishakh kp&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The oscillator clock should be selected whenever a tight tolerance (up to 0.1%) is required in the CAN bus timing. The crystal oscillator clock has better jitter performance than the peripheral clock.&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 23:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957727#M5281</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-08-12T23:35:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957728#M5282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;The CAN configuration shows only one Bit rate setting .As CAN FD supports different bit rates for data and Arbitration field,where I can set different bit rates?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;&lt;P&gt;Vishakh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 04:21:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957728#M5282</guid>
      <dc:creator>sreevishakhkp</dc:creator>
      <dc:date>2019-08-13T04:21:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957729#M5283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hi Sreevishakh kp &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;If you scroll down in that field, you can see the data phase too:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87652i4CEA75707688000E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jorge Alcala&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2019 15:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957729#M5283</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-08-14T15:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957730#M5284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Jorge&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Aug 2019 04:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957730#M5284</guid>
      <dc:creator>sreevishakhkp</dc:creator>
      <dc:date>2019-08-16T04:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957731#M5285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you suggest crystal oscillator part number suitable&amp;nbsp; for generating 5 Mbps baud rate please.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Aug 2019 04:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/957731#M5285</guid>
      <dc:creator>sreevishakhkp</dc:creator>
      <dc:date>2019-08-16T04:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 will support CANFD with 5000kbps?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/1479740#M8759</link>
      <description>&lt;P&gt;&lt;U&gt;Hi,&lt;/U&gt;&lt;/P&gt;&lt;P&gt;&lt;U&gt;&amp;nbsp; &amp;nbsp;Sorry to bother you. I am&amp;nbsp;a complete novicea and my boss keep telling me that if I can not let the CANFD communication run at 2Mhz with&amp;nbsp;&lt;SPAN&gt;osc of 8MHz and then it will be my problem.But I thought that it at least need an&amp;nbsp;osc of 12MHz.So can you just tell me how fast can the CANFD run with&amp;nbsp;osc of 8MHz?I'll be apreciate.&lt;/SPAN&gt;&lt;/U&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jun 2022 09:06:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32k144-will-support-CANFD-with-5000kbps/m-p/1479740#M8759</guid>
      <dc:creator>Andy_Pu</dc:creator>
      <dc:date>2022-06-24T09:06:58Z</dc:date>
    </item>
  </channel>
</rss>