<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: target processor settings not included in .args files</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953962#M5267</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Edgar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, you can manually fix the project files. you can open .cproject file from imported project in any editor (make sure that project is closed in IDE) and you need to find statement like this&amp;nbsp;&lt;SPAN&gt; &lt;/SPAN&gt;&amp;lt;option id="com.nxp.s32ds.cle.arm.mbs.arm32.bare.option.target.mcpu.cortex-m0plus842350448" (the number could be different). The value should be corrected to remove "&lt;SPAN&gt;cortex-m0plus&lt;/SPAN&gt;" (or "cortex-m4" correspondingly), so it will look like:&amp;nbsp;&lt;SPAN&gt;&amp;lt;option id="com.nxp.s32ds.cle.arm.mbs.arm32.bare.option.target.mcpu.842350448"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;after that you can reopen project and setting should start work normally.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Oct 2019 13:53:21 GMT</pubDate>
    <dc:creator>b13310</dc:creator>
    <dc:date>2019-10-03T13:53:21Z</dc:date>
    <item>
      <title>target processor settings not included in .args files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953958#M5263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using S32 Design Studio for ARM Version: 2018.R1 Build id: 180815.&lt;/P&gt;&lt;P&gt;I need to to do some setiings in&lt;/P&gt;&lt;P&gt;Project Settings -&amp;gt;C/C++ Build -&amp;gt;Settings-&amp;gt;Target Processor&lt;/P&gt;&lt;P&gt;I want to change toolchain default to some project specific settings.&lt;/P&gt;&lt;P&gt;After clean and then build the .args files do not contain the new settings.&lt;/P&gt;&lt;P&gt;Eg when I specify "cortex-m4" I expect the option "-mcpu=cortex-m4"&lt;/P&gt;&lt;P&gt;in the .args files.&lt;/P&gt;&lt;P&gt;What do I missed to do additionally that the options are correctls included?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 20:18:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953958#M5263</guid>
      <dc:creator>edgar_michel</dc:creator>
      <dc:date>2019-09-20T20:18:26Z</dc:date>
    </item>
    <item>
      <title>Re: target processor settings not included in .args files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953959#M5264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did some research&amp;nbsp; - and it looks that for example projects based on SDK can't be this settings changed (it is overwritten by example internal settings). When you create new project from scratch or use non SDK example - you can change this settings.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for report. I'll create bug ticket.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2019 07:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953959#M5264</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-09-23T07:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: target processor settings not included in .args files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953960#M5265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jiri,&lt;BR /&gt;thanks for the quick reply. Is there any way to patch this - eg patch a XML file?&lt;BR /&gt;I just want to set the default parameters.&lt;/P&gt;&lt;P&gt;Actually I need to add the required options to miscellaneous for compiler and linker.&lt;BR /&gt;However there are some inconsistencies.&lt;BR /&gt;Thanks Edgar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Sep 2019 20:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953960#M5265</guid>
      <dc:creator>edgar_michel</dc:creator>
      <dc:date>2019-09-23T20:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: target processor settings not included in .args files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953961#M5266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello Edgar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just to make sure - are you changing settings for the same build configuration where you check args file?&lt;/P&gt;&lt;P&gt;In general you can check what options would be generated on settings page for Compiler&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90348i04DD632ED7D1E92C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 18:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953961#M5266</guid>
      <dc:creator>b13310</dc:creator>
      <dc:date>2019-10-01T18:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: target processor settings not included in .args files</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953962#M5267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Edgar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, you can manually fix the project files. you can open .cproject file from imported project in any editor (make sure that project is closed in IDE) and you need to find statement like this&amp;nbsp;&lt;SPAN&gt; &lt;/SPAN&gt;&amp;lt;option id="com.nxp.s32ds.cle.arm.mbs.arm32.bare.option.target.mcpu.cortex-m0plus842350448" (the number could be different). The value should be corrected to remove "&lt;SPAN&gt;cortex-m0plus&lt;/SPAN&gt;" (or "cortex-m4" correspondingly), so it will look like:&amp;nbsp;&lt;SPAN&gt;&amp;lt;option id="com.nxp.s32ds.cle.arm.mbs.arm32.bare.option.target.mcpu.842350448"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;after that you can reopen project and setting should start work normally.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 13:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/target-processor-settings-not-included-in-args-files/m-p/953962#M5267</guid>
      <dc:creator>b13310</dc:creator>
      <dc:date>2019-10-03T13:53:21Z</dc:date>
    </item>
  </channel>
</rss>