<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: can't program S32 bootLoader example for mpc5748G in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953660#M5260</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri&lt;/P&gt;&lt;P&gt;you are great!&lt;/P&gt;&lt;P&gt;it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks allot&lt;/P&gt;&lt;P&gt;Dany&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jun 2019 09:24:29 GMT</pubDate>
    <dc:creator>dany_amsalem</dc:creator>
    <dc:date>2019-06-24T09:24:29Z</dc:date>
    <item>
      <title>can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953655#M5255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this topic has many info in the web yet&amp;nbsp; nothing help me to overcome this issue.&lt;/P&gt;&lt;P&gt;I'm using the DEV-KIT of mpc5748G chip and working on the bootLoader example, My first basic thing to do is to load this project RBF file into target and without any success.&lt;/P&gt;&lt;P&gt;i'm using the&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;DEBUG-OPENSDA-E200_Pemicro_v110.SDA&lt;/STRONG&gt;&lt;/EM&gt; in&amp;nbsp; target (according to others answer in the web).&lt;/P&gt;&lt;P&gt;trying to drag &amp;amp; drop RBF file into target during bootLader mode doesn't work as well&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any idea what i'm missing ? is it S32 IDE issue or PEmicro driver/app ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dumping below S32 Console prompts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1. Connection from port "53451" to 7224&lt;BR /&gt;Copyright 2018 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=OPENSDA -speed=5000 -port=´&lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xC Device detected. &lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&amp;amp;E\nxp_mpc5748g_1x32x1520k_cflash.pcp&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xC Device detected. &lt;BR /&gt;Initialized.&lt;BR /&gt; &lt;BR /&gt;;version 1.05, 06/26/2017, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [5748G_6080k]&lt;BR /&gt; &lt;BR /&gt;;device NXP, MPC5748G, 1x32x1520k, desc=CFlash&lt;BR /&gt; &lt;BR /&gt;;begin_cs device=$00F90000, length=$005F0000, ram=$40000000&lt;BR /&gt; &lt;BR /&gt;Loading programming algorithm ... &lt;BR /&gt; &lt;BR /&gt;WARNING - Selected .PCP file has been modified. CRC16 = $5A63 &lt;BR /&gt;Done.&lt;BR /&gt;Programming sequency is : erase, blank check, program, and verify {default} &lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ... &lt;BR /&gt;Error - no valid data in range of module.&lt;BR /&gt;CMD&amp;gt;EM&lt;BR /&gt; &lt;BR /&gt;Erasing.&lt;BR /&gt;Module has been erased.&lt;BR /&gt;CMD&amp;gt;PM&lt;BR /&gt; &lt;BR /&gt;Programming.&lt;BR /&gt;Processing Object File Data ... &lt;BR /&gt; &lt;BR /&gt;No data to program. &lt;BR /&gt; &lt;BR /&gt;. &lt;BR /&gt;Error during programming.&lt;BR /&gt;Error Programming flash of device &lt;BR /&gt;Error occured during Flash programming. &lt;BR /&gt; &lt;BR /&gt;Starting reset script (C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) ... &lt;BR /&gt;REM This script is compatible with MPC574xG devices. &lt;BR /&gt;REM Clean GPRs to remove residual data after using algorithm &lt;BR /&gt; &lt;BR /&gt;Reset script (C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&amp;amp;E\s32e200_mpc574xg.mac) completed. &lt;BR /&gt; &lt;BR /&gt;MPC574xG Device detected. &lt;BR /&gt;PE-ERROR: Error downloading to the device.&lt;BR /&gt;Disconnected from "127.0.0.1" via 127.0.0.1&lt;BR /&gt;Target Disconnected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2019 12:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953655#M5255</guid>
      <dc:creator>dany_amsalem</dc:creator>
      <dc:date>2019-06-20T12:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953656#M5256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;here is document related to RappID BL tool -&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-342287"&gt;https://community.nxp.com/docs/DOC-342287&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is for MPC5744p, but principle is the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jun 2019 12:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953656#M5256</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-06-20T12:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953657#M5257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unfortunately, it doesn't work. I have used the attached project (hello world...) and nothing, loading process at console showed nothing.&lt;/P&gt;&lt;P&gt;trying with RappID BL tool results the same (communication timeout).&lt;/P&gt;&lt;P&gt;any idea ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some questions:&lt;/P&gt;&lt;P&gt;1. Is there a way to validate that&amp;nbsp;&lt;SPAN&gt;RappID BL tool is working and all drivers are OK ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2. Do you have bootLoader 5748G project that works ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;3. Would you link me the right RappID BL tool, (i found several of them) which one is suitable for the mpc5748G ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Dany&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jun 2019 15:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953657#M5257</guid>
      <dc:creator>dany_amsalem</dc:creator>
      <dc:date>2019-06-23T15:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953658#M5258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri&lt;/P&gt;&lt;P&gt;Is it possible to convert RBF file into ELF file format ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dany&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Jun 2019 15:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953658#M5258</guid>
      <dc:creator>dany_amsalem</dc:creator>
      <dc:date>2019-06-23T15:19:53Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953659#M5259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I figured out that you are using wrong programming algorithm. RappID bootloader is located in hsmcode flash part. You need to use alternative algorithm:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89529i5E0C72938344D4B5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;.pcp files are by default located in&amp;nbsp;&lt;/P&gt;&lt;P&gt;c:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.8.3.201812312131\win32\gdi\P&amp;amp;E\&lt;/P&gt;&lt;P&gt;folder.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 08:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953659#M5259</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-06-24T08:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953660#M5260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri&lt;/P&gt;&lt;P&gt;you are great!&lt;/P&gt;&lt;P&gt;it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks allot&lt;/P&gt;&lt;P&gt;Dany&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 09:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/953660#M5260</guid>
      <dc:creator>dany_amsalem</dc:creator>
      <dc:date>2019-06-24T09:24:29Z</dc:date>
    </item>
    <item>
      <title>Re: can't program S32 bootLoader example for mpc5748G</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/1307278#M7641</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am using Rappid BL Tool software to upgrade MPC5777C through serial port. I have been upgraded successfully, but I cannot start it and it stays in the bootloader &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jul 2021 03:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/can-t-program-S32-bootLoader-example-for-mpc5748G/m-p/1307278#M7641</guid>
      <dc:creator>曹培亮</dc:creator>
      <dc:date>2021-07-14T03:03:58Z</dc:date>
    </item>
  </channel>
</rss>