<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Adding existing source file to a project</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920952#M5053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.&amp;nbsp; then it showed up and became part of the build.&amp;nbsp; thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Oct 2019 13:58:36 GMT</pubDate>
    <dc:creator>danielkageff</dc:creator>
    <dc:date>2019-10-16T13:58:36Z</dc:date>
    <item>
      <title>Adding existing source file to a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920950#M5051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am using S32 Design Studio for ARM 2018.R1 and have created an application project.&amp;nbsp; I want to add some existing source files to the project but can't figure out how to do it.&amp;nbsp; How is it done?&amp;nbsp; Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 19:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920950#M5051</guid>
      <dc:creator>danielkageff</dc:creator>
      <dc:date>2019-10-15T19:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: Adding existing source file to a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920951#M5052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can for example drag and drop your source file or simply copy your sources into workspace/Project/sources and include folder. There is nothing special about it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91650iF6DFB81EF792BF59/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2019 12:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920951#M5052</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-10-16T12:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: Adding existing source file to a project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920952#M5053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I did that, but didn't see the file in Sources until I figured out that I had to right-click on the folder and selet 'Refresh'.&amp;nbsp; then it showed up and became part of the build.&amp;nbsp; thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2019 13:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Adding-existing-source-file-to-a-project/m-p/920952#M5053</guid>
      <dc:creator>danielkageff</dc:creator>
      <dc:date>2019-10-16T13:58:36Z</dc:date>
    </item>
  </channel>
</rss>