<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Type bool can not be solved in 5748g</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915700#M5004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried your project, and it works on my machine without any issue. So, you can try to create new workspace (sometime it helps) or re-install S32DS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jul 2019 10:15:47 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2019-07-18T10:15:47Z</dc:date>
    <item>
      <title>Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915695#M4999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The program I used is the example project with the name of hsm_freertos_mpc5748g. When I try to debug the project, the type bool can not be resolved. I used to method which is mentioned in the&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/472056"&gt;https://community.nxp.com/thread/472056&lt;/A&gt;, it does not works.&amp;nbsp;&amp;nbsp;I have no idea to solve this issue.....And how to solve it ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91108i5E687A5B61D6415C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jul 2019 13:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915695#M4999</guid>
      <dc:creator>961271210</dc:creator>
      <dc:date>2019-07-12T13:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915696#M5000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which C library are you using - EWL or NewLib? Can you please share your project?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 07:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915696#M5000</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-07-16T07:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915697#M5001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where can I find the C library in the S32DS?&amp;nbsp; I do not find it. The project which I used is the example project from S32, it name is hsm_freetos_mpc5748g, I import the example project from S32 directly and I do not change anything in it. I do not know why I can not upload my project, there is not an option can do that.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jupeng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 08:41:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915697#M5001</guid>
      <dc:creator>961271210</dc:creator>
      <dc:date>2019-07-16T08:41:41Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915698#M5002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you can upload project by Use advanced editor option:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65260i4769362952801CB6/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is probably something wrong with your project settings/S32DS Installation. bool is defined in stdbool.h header file - based on used C library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find which one is used in Project Properties (right click on project name) -&amp;gt; Properties -&amp;gt; Settings -&amp;gt; Target processor:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65079i699D368D0B8DBE5A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 08:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915698#M5002</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-07-16T08:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915699#M5003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the C library which I used. And I upload my project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65364iBAF50F08110B3E73/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jupeng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 09:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915699#M5003</guid>
      <dc:creator>961271210</dc:creator>
      <dc:date>2019-07-16T09:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915700#M5004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried your project, and it works on my machine without any issue. So, you can try to create new workspace (sometime it helps) or re-install S32DS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 10:15:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915700#M5004</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-07-18T10:15:47Z</dc:date>
    </item>
    <item>
      <title>Re: Type bool can not be solved in 5748g</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915701#M5005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I re-install S32 in other path and get the following image, it seems there are not any issues. But in this project, I cannot receive any messages from serial port. I wonder if the right result is that the board will send a sentence by serial port ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81930i8135D3413C7BF15D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jupeng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 14:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Type-bool-can-not-be-solved-in-5748g/m-p/915701#M5005</guid>
      <dc:creator>961271210</dc:creator>
      <dc:date>2019-07-18T14:37:46Z</dc:date>
    </item>
  </channel>
</rss>