<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe-Flash issue with S32 Flash tool for S32V234</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Re-Flash-issue-with-S32-Flash-tool-for-S32V234/m-p/905736#M4913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to flash u-boot into eMMC and I got the issue that fail to load algorithm and device file when I reprogramming it.&lt;/P&gt;&lt;P&gt;There was no issue to flash u-boot at the first time, however, the issue was occurred on second time, it means that flash tool doesn't work after running u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain the reason why it doesn't work after running u-boot and solution?&lt;/P&gt;&lt;P&gt;I know the workaround in case of using EVB&amp;nbsp;with switching boot device jumper to&amp;nbsp;avoid booting, however, customer board has no jumper to prevent booting.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80201i7EAE57325BDA8DC8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that it is same issue when running the demo&amp;nbsp;sdhc_fatfs_s32v234. The demo doesn't work if u-boot is in the SDCARD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Please explain root cause of the issue.&lt;/P&gt;&lt;P&gt;2. How can I modify the&amp;nbsp;&lt;SPAN&gt;sdhc_fatfs_s32v234 demo to run with SDCARD u-boot inside.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;John Yoo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Apr 2019 07:00:14 GMT</pubDate>
    <dc:creator>johnyoo</dc:creator>
    <dc:date>2019-04-23T07:00:14Z</dc:date>
    <item>
      <title>Re-Flash issue with S32 Flash tool for S32V234</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Re-Flash-issue-with-S32-Flash-tool-for-S32V234/m-p/905736#M4913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to flash u-boot into eMMC and I got the issue that fail to load algorithm and device file when I reprogramming it.&lt;/P&gt;&lt;P&gt;There was no issue to flash u-boot at the first time, however, the issue was occurred on second time, it means that flash tool doesn't work after running u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you explain the reason why it doesn't work after running u-boot and solution?&lt;/P&gt;&lt;P&gt;I know the workaround in case of using EVB&amp;nbsp;with switching boot device jumper to&amp;nbsp;avoid booting, however, customer board has no jumper to prevent booting.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80201i7EAE57325BDA8DC8/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that it is same issue when running the demo&amp;nbsp;sdhc_fatfs_s32v234. The demo doesn't work if u-boot is in the SDCARD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Please explain root cause of the issue.&lt;/P&gt;&lt;P&gt;2. How can I modify the&amp;nbsp;&lt;SPAN&gt;sdhc_fatfs_s32v234 demo to run with SDCARD u-boot inside.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;John Yoo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 07:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Re-Flash-issue-with-S32-Flash-tool-for-S32V234/m-p/905736#M4913</guid>
      <dc:creator>johnyoo</dc:creator>
      <dc:date>2019-04-23T07:00:14Z</dc:date>
    </item>
  </channel>
</rss>