<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Questions about CAN RX signal reception failure</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895463#M4838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alexandru Nan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you as for answer.&lt;/P&gt;&lt;P&gt;We have applied an external 12V power to the SBC transceiver.&lt;BR /&gt;We also checked that the signal was normally transferred to the CAN H / L pin, MCU CAN TX/RX pin using the oscilloscope.&lt;BR /&gt;However, the example code does not recognize the RX signal.&lt;/P&gt;&lt;P&gt;I suspect the ID you mentioned.(MASTER / SLAVE)&lt;BR /&gt;Could you please explain in more detail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 May 2019 06:50:03 GMT</pubDate>
    <dc:creator>jm_shin</dc:creator>
    <dc:date>2019-05-21T06:50:03Z</dc:date>
    <item>
      <title>Questions about CAN RX signal reception failure</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895461#M4836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used CANoe to transmit the CAN signal to the EVB board.&lt;BR /&gt;However, CAN signal was not received in EVB.&lt;BR /&gt;The example code I used is can_pal_s32k144 of 'S32K1xx RTM SDK v3.0.0 Example Project'&lt;BR /&gt;And the sample code was tested by flashing without modification.&lt;BR /&gt;CANoe carries the CAN signal but the status does not change in the FLEXCAN_DRV_GetTransferStatus function.&lt;BR /&gt;How do I receive the RX signal from the EVB board?&lt;BR /&gt;How can I check whether CAN signal is received from EVB board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 00:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895461#M4836</guid>
      <dc:creator>jm_shin</dc:creator>
      <dc:date>2019-05-16T00:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about CAN RX signal reception failure</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895462#M4837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CAN works through a SBC transceiver, in order to activate SBC, you need to power externally the EVB board with 12V on J16.&lt;/P&gt;&lt;P&gt;The signals can be received on J13.1 CAN_Hi and J13.2 CAN_Lo.&lt;/P&gt;&lt;P&gt;The example uses CAN FD frame type with Arbitration Phase 500kbps and Data Phase 1000Kbps.&lt;/P&gt;&lt;P&gt;And depends how you configured the FW from the board if you selected&amp;nbsp;MASTER the ID accepted is 2 if is SLAVE then the ID accepted is 1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Alexandru Nan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 13:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895462#M4837</guid>
      <dc:creator>alexandrunan</dc:creator>
      <dc:date>2019-05-20T13:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about CAN RX signal reception failure</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895463#M4838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alexandru Nan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you as for answer.&lt;/P&gt;&lt;P&gt;We have applied an external 12V power to the SBC transceiver.&lt;BR /&gt;We also checked that the signal was normally transferred to the CAN H / L pin, MCU CAN TX/RX pin using the oscilloscope.&lt;BR /&gt;However, the example code does not recognize the RX signal.&lt;/P&gt;&lt;P&gt;I suspect the ID you mentioned.(MASTER / SLAVE)&lt;BR /&gt;Could you please explain in more detail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 06:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895463#M4838</guid>
      <dc:creator>jm_shin</dc:creator>
      <dc:date>2019-05-21T06:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about CAN RX signal reception failure</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895464#M4839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;By default the example came configured as MASTER.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Use this define to specify if the application runs as master or slave */&lt;BR /&gt;#define MASTER&lt;BR /&gt;/* #define SLAVE */&lt;/P&gt;&lt;P&gt;/* Definition of the TX and RX message buffers depending on the bus role */&lt;BR /&gt;#if defined(MASTER)&lt;BR /&gt; #define TX_MAILBOX (1UL)&lt;BR /&gt; #define TX_MSG_ID (1UL)&lt;BR /&gt; #define RX_MAILBOX (0UL)&lt;BR /&gt; #define RX_MSG_ID (2UL)&lt;BR /&gt;#elif defined(SLAVE)&lt;BR /&gt; #define TX_MAILBOX (0UL)&lt;BR /&gt; #define TX_MSG_ID (2UL)&lt;BR /&gt; #define RX_MAILBOX (1UL)&lt;BR /&gt; #define RX_MSG_ID (1UL)&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you used the default configuration then the expected frame should be CAN_FD with ID 2 and payload 1 byte with data[0] as 0 or 1.&lt;/P&gt;&lt;P&gt;To check if you receive something pres one of the buttons and you should receive an FD frame with ID 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 09:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Questions-about-CAN-RX-signal-reception-failure/m-p/895464#M4839</guid>
      <dc:creator>alexandrunan</dc:creator>
      <dc:date>2019-05-21T09:10:08Z</dc:date>
    </item>
  </channel>
</rss>