<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32R274rruevb</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32R274rruevb/m-p/885168#M4694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, the Daughter board can be used as standalone EVB. You need external power supply 5V, 3.3V and 1.25V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no OpenSDA debug probe present on board. Mini USB connector is used as RS232 over USB. You have to use external debug probe - PE Micro Multilink FX for example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Mar 2019 08:18:34 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2019-03-25T08:18:34Z</dc:date>
    <item>
      <title>S32R274rruevb</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32R274rruevb/m-p/885167#M4693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have ordered the part S32R274RRUEVB (daughter board only). I would like to know:&lt;/P&gt;&lt;P&gt;(1) Is it possible to load program / run / debug use the daughter board only?&lt;/P&gt;&lt;P&gt;(2) If it is, what connection is necessary between daughter board and PC? For example, from a question (&lt;A _jive_internal="true" href="https://community.nxp.com/thread/480632?q=S32R274rruevb"&gt;https://community.nxp.com/message/1037532?q=S32R274rruevb&lt;/A&gt;) I knew that PE Micro USB Multilink is recommended for connection, but what Micro USB Multilink do?&lt;/P&gt;&lt;P&gt;(3) Furthermore,&amp;nbsp;is a USB mini cable able to meet my requirements(debug/load/run), or if I could do it with a USB mini calbe plus a JTAG debugger?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2019 01:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32R274rruevb/m-p/885167#M4693</guid>
      <dc:creator>220141204</dc:creator>
      <dc:date>2019-03-25T01:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32R274rruevb</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32R274rruevb/m-p/885168#M4694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, the Daughter board can be used as standalone EVB. You need external power supply 5V, 3.3V and 1.25V.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no OpenSDA debug probe present on board. Mini USB connector is used as RS232 over USB. You have to use external debug probe - PE Micro Multilink FX for example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Mar 2019 08:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32R274rruevb/m-p/885168#M4694</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-03-25T08:18:34Z</dc:date>
    </item>
  </channel>
</rss>