<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IRQ with processor expert in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/IRQ-with-processor-expert/m-p/880362#M4589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello expert,&lt;/P&gt;&lt;P style="margin-left: 24.0pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;My requirement is that : when pin2 of Port B input 0, then a gpio interrupt will be triggered. I do the configuration as following fig:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: 24.0pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77020i665538A8328BCC46/image-size/large?v=v2&amp;amp;px=999" title="setting_1.bmp" alt="setting_1.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;I do not understand where can I set the IRQ callback function? the following codes are used for the whole pins of Port B, but I only want to pin2 of Port B to trigger interrupt, other pins of Port B are ignored. How can I do to set the pin2 of port B interrupt?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76938i6DCED5ACC5AAAA4C/image-size/large?v=v2&amp;amp;px=999" title="setting_2.bmp" alt="setting_2.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So I met the problem : how can I generate &amp;nbsp;a gpio interrupt of one pin with processor expert of S32DS&lt;/SPAN&gt; &lt;SPAN style="font-size: 12.0pt;"&gt;？&lt;/SPAN&gt; &lt;SPAN style="font-size: 12.0pt;"&gt;&lt;SPAN&gt;Could you help me again? Thank you very much!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2019 09:32:42 GMT</pubDate>
    <dc:creator>zhaoyanling</dc:creator>
    <dc:date>2019-02-21T09:32:42Z</dc:date>
    <item>
      <title>IRQ with processor expert</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/IRQ-with-processor-expert/m-p/880362#M4589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello expert,&lt;/P&gt;&lt;P style="margin-left: 24.0pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;My requirement is that : when pin2 of Port B input 0, then a gpio interrupt will be triggered. I do the configuration as following fig:&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-left: 24.0pt;"&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/77020i665538A8328BCC46/image-size/large?v=v2&amp;amp;px=999" title="setting_1.bmp" alt="setting_1.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;I do not understand where can I set the IRQ callback function? the following codes are used for the whole pins of Port B, but I only want to pin2 of Port B to trigger interrupt, other pins of Port B are ignored. How can I do to set the pin2 of port B interrupt?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76938i6DCED5ACC5AAAA4C/image-size/large?v=v2&amp;amp;px=999" title="setting_2.bmp" alt="setting_2.bmp" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So I met the problem : how can I generate &amp;nbsp;a gpio interrupt of one pin with processor expert of S32DS&lt;/SPAN&gt; &lt;SPAN style="font-size: 12.0pt;"&gt;？&lt;/SPAN&gt; &lt;SPAN style="font-size: 12.0pt;"&gt;&lt;SPAN&gt;Could you help me again? Thank you very much!&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 09:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/IRQ-with-processor-expert/m-p/880362#M4589</guid>
      <dc:creator>zhaoyanling</dc:creator>
      <dc:date>2019-02-21T09:32:42Z</dc:date>
    </item>
  </channel>
</rss>