<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic the system will be reset when run RAMCODE in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/the-system-will-be-reset-when-run-RAMCODE/m-p/877446#M4562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Csec Driver and Flash Driver, some function is placed in RAM. Use "START_FUNCTION_DEFINITION_RAMSECTION" and&amp;nbsp;END_FUNCTION_DEFINITION_RAMSECTION.&lt;/P&gt;&lt;P&gt;for example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20842iD6E426A4EE257E1D/image-size/large?v=v2&amp;amp;px=999" title="Snipaste_2019-01-16_12-05-53.png" alt="Snipaste_2019-01-16_12-05-53.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The csec init driver will start the system tick.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21013i349761B050C92557/image-size/large?v=v2&amp;amp;px=999" title="Snipaste_2019-01-16_12-13-09.png" alt="Snipaste_2019-01-16_12-13-09.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I init the csec driver, then call some cesc or flash function that need run RAMCODE. when the code run to the RAMCODE, the system will be reset.&lt;/P&gt;&lt;P&gt;if I disable the system tick, those function will be run succeed, and there is no system reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know why it happened. I don't know why the system tick will&amp;nbsp; impact the ramcode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody can explain the theory or reason to me?&lt;/P&gt;&lt;P&gt;I don't know disbale the system tick will really run those function succeed every time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jan 2019 04:27:55 GMT</pubDate>
    <dc:creator>香龙朱</dc:creator>
    <dc:date>2019-01-16T04:27:55Z</dc:date>
    <item>
      <title>the system will be reset when run RAMCODE</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/the-system-will-be-reset-when-run-RAMCODE/m-p/877446#M4562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Csec Driver and Flash Driver, some function is placed in RAM. Use "START_FUNCTION_DEFINITION_RAMSECTION" and&amp;nbsp;END_FUNCTION_DEFINITION_RAMSECTION.&lt;/P&gt;&lt;P&gt;for example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20842iD6E426A4EE257E1D/image-size/large?v=v2&amp;amp;px=999" title="Snipaste_2019-01-16_12-05-53.png" alt="Snipaste_2019-01-16_12-05-53.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The csec init driver will start the system tick.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21013i349761B050C92557/image-size/large?v=v2&amp;amp;px=999" title="Snipaste_2019-01-16_12-13-09.png" alt="Snipaste_2019-01-16_12-13-09.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I init the csec driver, then call some cesc or flash function that need run RAMCODE. when the code run to the RAMCODE, the system will be reset.&lt;/P&gt;&lt;P&gt;if I disable the system tick, those function will be run succeed, and there is no system reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know why it happened. I don't know why the system tick will&amp;nbsp; impact the ramcode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody can explain the theory or reason to me?&lt;/P&gt;&lt;P&gt;I don't know disbale the system tick will really run those function succeed every time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 04:27:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/the-system-will-be-reset-when-run-RAMCODE/m-p/877446#M4562</guid>
      <dc:creator>香龙朱</dc:creator>
      <dc:date>2019-01-16T04:27:55Z</dc:date>
    </item>
    <item>
      <title>Re: the system will be reset when run RAMCODE</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/the-system-will-be-reset-when-run-RAMCODE/m-p/877447#M4563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;this issue may be the same reason as&amp;nbsp;&lt;A href="https://community.nxp.com/thread/496524"&gt;https://community.nxp.com/thread/496524&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anybody can give me some tips?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 08:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/the-system-will-be-reset-when-run-RAMCODE/m-p/877447#M4563</guid>
      <dc:creator>香龙朱</dc:creator>
      <dc:date>2019-02-26T08:56:08Z</dc:date>
    </item>
  </channel>
</rss>