<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561125#M452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to port your code to S32DS next week.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just one question. Are you able to load default project for MPC5644A to your microcontroller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Aug 2016 11:55:36 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2016-08-26T11:55:36Z</dc:date>
    <item>
      <title>MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561124#M451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've porting CW10.6 project into S32DS and it use MPC5644A&lt;/P&gt;&lt;P&gt;then CW10.6 it can be work but S32DS can not work&lt;/P&gt;&lt;P&gt;error message is here and attachment is source code&lt;/P&gt;&lt;P&gt;when i run this code i always find "&lt;STRONG&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;0x00000004 in RCHW2 ()&lt;/STRONG&gt;" this problem, then S32DS stop debug&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could someone can provide a MPC5644A moounted on S32DS example?&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;GNU gdb (GDB) 7.8.2&lt;BR /&gt;Copyright (C) 2014 Free Software Foundation, Inc.&lt;BR /&gt;&lt;SPAN&gt;License GPLv3+: GNU GPL version 3 or later &amp;lt;&lt;/SPAN&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fgnu.org%2Flicenses%2Fgpl.html"&gt;http://gnu.org/licenses/gpl.html&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;This is free software: you are free to change and redistribute it.&lt;BR /&gt;There is NO WARRANTY, to the extent permitted by law. Type "show copying"&lt;BR /&gt;and "show warranty" for details.&lt;BR /&gt;This GDB was configured as "--host=i686-mingw32 --target=powerpc-eabivle".&lt;BR /&gt;Type "show configuration" for configuration details.&lt;BR /&gt;For bug reporting instructions, please see:&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoftware%2Fgdb%2Fbugs%2F"&gt;http://www.gnu.org/software/gdb/bugs/&lt;/A&gt;&lt;SPAN&gt;&amp;gt;.&lt;/SPAN&gt;&lt;BR /&gt;Find the GDB manual and other documentation resources online at:&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.gnu.org%2Fsoftware%2Fgdb%2Fdocumentation%2F"&gt;http://www.gnu.org/software/gdb/documentation/&lt;/A&gt;&lt;SPAN&gt;&amp;gt;.&lt;/SPAN&gt;&lt;BR /&gt;For help, type "help".&lt;BR /&gt;Type "apropos word" to search for commands related to "word".&lt;BR /&gt;monitor preserve0 0&lt;BR /&gt;monitor selectcore 0&lt;BR /&gt;Warning: the current language does not match this frame.&lt;BR /&gt;continue&lt;BR /&gt;Continuing.&lt;BR /&gt;Note: automatically using hardware breakpoints for read-only addresses.&lt;/P&gt;&lt;P&gt;Temporary breakpoint 1, main () at ../src/main.c:270&lt;BR /&gt;270 HW_init();&lt;BR /&gt;set architecture powerpc:vle&lt;BR /&gt;The target architecture is assumed to be powerpc:vle&lt;BR /&gt;No breakpoint number 2.&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000004 in RCHW2 ()&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339036"&gt;main.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 17:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561124#M451</guid>
      <dc:creator>alexhuang5367</dc:creator>
      <dc:date>2016-08-25T17:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561125#M452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to port your code to S32DS next week.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just one question. Are you able to load default project for MPC5644A to your microcontroller?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2016 11:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561125#M452</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-26T11:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561126#M453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Martin&lt;/P&gt;&lt;P&gt;Thank you so much.&lt;/P&gt;&lt;P&gt;Yes, I've used the default head file and source code in the project.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If you have any questions or whole project, please do not hesitate to contact me&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Sincerely,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alex&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2016 22:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561126#M453</guid>
      <dc:creator>alexhuang5367</dc:creator>
      <dc:date>2016-08-26T22:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561127#M454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created simple example based on the code you shared in the first post. I am able to load to to microcontroller flash memory and also RAM memory. It is important to use S32 Design Studio version 1.1 (the older version does not support MPC5644A).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which debug probe you use for loading the code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Import the project I created and try to load it to your microcontroller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: I did not implement interrupt handler, so PIT interrupt does not work, but you should be able to debug the rest of the code. Do not forget you have to use only debug icon for loading the code. Run icon does not work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 11:06:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561127#M454</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-29T11:06:13Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561128#M455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is my problem, when i open the PIT interrupt&lt;/P&gt;&lt;P&gt;I'm so confuse about the error message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000004 in RCHW2 ()&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000006 in RCHW2 ()&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000004 in RCHW2 ()&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000006 in RCHW2 ()&lt;/P&gt;&lt;P&gt;Program received signal SIGTRAP, Trace/breakpoint trap.&lt;BR /&gt;0x00000004 in RCHW2 ()&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2799i938862BAFF770117/image-size/large?v=v2&amp;amp;px=999" title="STUCK.PNG" alt="STUCK.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This page just show you what debug prob i use&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2852i69EBA3ADD129BA56/image-size/large?v=v2&amp;amp;px=999" title="debuger.PNG" alt="debuger.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2016 14:55:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561128#M455</guid>
      <dc:creator>alexhuang5367</dc:creator>
      <dc:date>2016-08-29T14:55:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561129#M456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found the issue. In MPC56xx__Interrupts_Init.c file is function InitIVORS, which is not compiled, because neither symbol E200Z4 nor symbol E200Z7 is defined. If you use e200z4 core, it is necessary to initialize IVOR registers (which is not done in the project).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So the simple workaround is to define symbol E200Z4 for compiler. Open project properties, open tab Symbols in compiler sub-menu and add new symbol. Recompile the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now it will work.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3059iCFFBFDC592E2D115/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 06:48:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561129#M456</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-30T06:48:09Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561130#M457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;AWESOME!!&lt;/P&gt;&lt;P&gt;Thank your so much for your help, I really appreciate it.&lt;/P&gt;&lt;P&gt;How did you find it? Compare with MPC574x or MPC5643 project or Assembly code?&lt;/P&gt;&lt;P&gt;I really want to know that, if you convenience please tell me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2016 16:10:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561130#M457</guid>
      <dc:creator>alexhuang5367</dc:creator>
      <dc:date>2016-08-30T16:10:12Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644A mounted on S32DS can not open interrupt S32DS is a big bug IDE?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561131#M458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not compare any project. I took the project I shared here and I loaded it to microcontroller using Lauterbach debugger. Then I stepped through xcptn_xmpl function. I saw there is no code in InitIVORS function. From my knowledge of e200z4 core I know, I have to initialize single IVOR registers with correct values and that is it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had opened MPC56xx_interrupt_Init.c file and I found there is conditional compilation and neither&amp;nbsp;E200Z4 symbol nor&amp;nbsp;E200Z7 symbol is defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have escalated this issue to appropriate team. So it should be fixed in next S32DS release.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any other question, please feel free to write me back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 08:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/MPC5644A-mounted-on-S32DS-can-not-open-interrupt-S32DS-is-a-big/m-p/561131#M458</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-08-31T08:25:05Z</dc:date>
    </item>
  </channel>
</rss>