<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studioのトピック1RF_4Antenna Demo with S32R274 and TEF810X</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/1RF-4Antenna-Demo-with-S32R274-and-TEF810X/m-p/869015#M4467</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to execute 1RF_4Antenna_Demo with TEF810X and S32R274 RRU Board.&lt;/P&gt;&lt;P&gt;I followed the reference manual given in Docs folder as well as the description file available with the example project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen that the example project has required header file for RFE setup. But the AppRfeInit() function in main_c1.c file is written only for MR3003.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the same example project is compatible with TEF810X?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;If yes, How to execute it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;If no, can you provide other demo project for the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sushant Gosavi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 05:38:09 GMT</pubDate>
    <dc:creator>sushant_sg</dc:creator>
    <dc:date>2019-01-11T05:38:09Z</dc:date>
    <item>
      <title>1RF_4Antenna Demo with S32R274 and TEF810X</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/1RF-4Antenna-Demo-with-S32R274-and-TEF810X/m-p/869015#M4467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to execute 1RF_4Antenna_Demo with TEF810X and S32R274 RRU Board.&lt;/P&gt;&lt;P&gt;I followed the reference manual given in Docs folder as well as the description file available with the example project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have seen that the example project has required header file for RFE setup. But the AppRfeInit() function in main_c1.c file is written only for MR3003.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the same example project is compatible with TEF810X?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;If yes, How to execute it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;If no, can you provide other demo project for the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Sushant Gosavi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 05:38:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/1RF-4Antenna-Demo-with-S32R274-and-TEF810X/m-p/869015#M4467</guid>
      <dc:creator>sushant_sg</dc:creator>
      <dc:date>2019-01-11T05:38:09Z</dc:date>
    </item>
  </channel>
</rss>