<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 ICC-LINUX-CAN</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/ICC-LINUX-CAN/m-p/865227#M4426</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I totally have two questions about S32V234 .&lt;/P&gt;&lt;P&gt;One is how to flash the M4 code using S32DS and where the code would be stored to ?&lt;/P&gt;&lt;P&gt;Another one is that I need a demo which is used for inter core communication between M4 running on bareboard and A53 running on linux ,it's looks pretty much like following picture shows :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="11.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72300i93184983441C8C1E/image-size/large?v=v2&amp;amp;px=999" role="button" title="11.PNG" alt="11.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any information related is needed for sure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2019 08:09:57 GMT</pubDate>
    <dc:creator>frank_feng</dc:creator>
    <dc:date>2019-02-15T08:09:57Z</dc:date>
    <item>
      <title>ICC-LINUX-CAN</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ICC-LINUX-CAN/m-p/865227#M4426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I totally have two questions about S32V234 .&lt;/P&gt;&lt;P&gt;One is how to flash the M4 code using S32DS and where the code would be stored to ?&lt;/P&gt;&lt;P&gt;Another one is that I need a demo which is used for inter core communication between M4 running on bareboard and A53 running on linux ,it's looks pretty much like following picture shows :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="11.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72300i93184983441C8C1E/image-size/large?v=v2&amp;amp;px=999" role="button" title="11.PNG" alt="11.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any information related is needed for sure.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 08:09:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ICC-LINUX-CAN/m-p/865227#M4426</guid>
      <dc:creator>frank_feng</dc:creator>
      <dc:date>2019-02-15T08:09:57Z</dc:date>
    </item>
    <item>
      <title>Re: ICC-LINUX-CAN</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ICC-LINUX-CAN/m-p/865228#M4427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;Have you find any solution about that ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;appreciate if you can share it .&lt;/P&gt;&lt;P&gt;Thx!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 02:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ICC-LINUX-CAN/m-p/865228#M4427</guid>
      <dc:creator>447825937</dc:creator>
      <dc:date>2019-07-31T02:06:06Z</dc:date>
    </item>
  </channel>
</rss>