<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: library's setting in the projectinfo.xml doesn't work in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861513#M4387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case importing/exporting library settings makes sense. I'll create ticket for that. Thank you for your report.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2019 05:13:47 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2019-01-10T05:13:47Z</dc:date>
    <item>
      <title>library's setting in the projectinfo.xml doesn't work</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861509#M4383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;I'm having a problem importing projectinfo.xml file into S32 Design Studio.&lt;/P&gt;&lt;P&gt;In the projectinfo.xml file, I tried to use libraries with the settings as showed in the following picture.&lt;/P&gt;&lt;P&gt;The library file is mpc.a.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71764i6E7EED85D8C9654A/image-size/large?v=v2&amp;amp;px=999" title="XML.png" alt="XML.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But after importing xml file , all configurations works but the library's configuration.&lt;/P&gt;&lt;P&gt;So I have to mannually add the library's name in order to compile the project successfully.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71732iCF1954B6B1B42D5C/image-size/large?v=v2&amp;amp;px=999" title="properties.png" alt="properties.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have also tried to export the projectinfo.xml from an existing project with the right library settings.&lt;/P&gt;&lt;P&gt;But there is no "-l:mpc.a"&amp;nbsp; in the exported XML file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything wrong with my XML file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;Laura&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 02:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861509#M4383</guid>
      <dc:creator>liuww_fnst</dc:creator>
      <dc:date>2019-01-09T02:54:34Z</dc:date>
    </item>
    <item>
      <title>Re: library's setting in the projectinfo.xml doesn't work</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861510#M4384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it seems that export/import project settings doesn't include all options - including libraries and library paths. I'll do more investigation and if it is a bug, I'll create ticket for it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a workaround you can add your libraries manually in project properties:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71968i5D8C79D23DFFC459/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 06:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861510#M4384</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-01-09T06:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: library's setting in the projectinfo.xml doesn't work</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861511#M4385</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try find out for what purpose can be projectinfo.xml used - but the only suitable use case which I found is transfer S32DS ARM project into IAR workbench.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, the question is, what you are trying to do with projectinfo.xml? If you like to import existing project into workspace - you can import it directly:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76542iFF91E28CA959AFE2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76577i88CCD84AABE1DA17/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This will import project with all dependencies.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 14:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861511#M4385</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-01-09T14:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: library's setting in the projectinfo.xml doesn't work</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861512#M4386</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks very much for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the projectinfo.xml, I just want to import the code generated by the matlab to S32 Design Studio without any mannual configuration.&lt;BR /&gt;The generated code only contains source files.So I tried to set the project properties using the projectinfo.xml.&lt;BR /&gt;If it works , after importing the projectinfo.xml, I can directly compile the project without any configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Laura&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 00:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861512#M4386</guid>
      <dc:creator>liuww_fnst</dc:creator>
      <dc:date>2019-01-10T00:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: library's setting in the projectinfo.xml doesn't work</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861513#M4387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in this case importing/exporting library settings makes sense. I'll create ticket for that. Thank you for your report.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 05:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/library-s-setting-in-the-projectinfo-xml-doesn-t-work/m-p/861513#M4387</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2019-01-10T05:13:47Z</dc:date>
    </item>
  </channel>
</rss>