<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flash Multiple S32K144 Boards At Once? in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848262#M4164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already tested flashing two boards simultaneous. Further experiments/testing with OpenSDA and more boards is up to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Oct 2018 17:19:26 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2018-10-02T17:19:26Z</dc:date>
    <item>
      <title>Flash Multiple S32K144 Boards At Once?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848258#M4160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1- I have multiple S32K144EVB boards connected to my PC and I wanted to flash the same SW project on all boards at the same time, either in parallel or one after the other automatically. Is it possible to achieve this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2- Also if I need to flash different SW's to different boards, is there a way to automate this process with one button click?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. I am using the standard PEMicro over OpenSDA to flash/debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 07:59:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848258#M4160</guid>
      <dc:creator>mahmoudsherrah</dc:creator>
      <dc:date>2018-09-20T07:59:06Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Multiple S32K144 Boards At Once?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848259#M4161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Sep 2018 10:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848259#M4161</guid>
      <dc:creator>mahmoudsherrah</dc:creator>
      <dc:date>2018-09-29T10:41:21Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Multiple S32K144 Boards At Once?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848260#M4162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the OpenSDA is not designed for multiple flashing. You can flash two boards - just by connecting JTAG between two boards. The "master" board is connected to PC via OpenSDA.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 15:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848260#M4162</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-10-02T15:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Multiple S32K144 Boards At Once?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848261#M4163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So flashing the master board would automatically flash the other one? Do you have an idea if this works for more than 2 boards?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 15:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848261#M4163</guid>
      <dc:creator>mahmoudsherrah</dc:creator>
      <dc:date>2018-10-02T15:35:35Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Multiple S32K144 Boards At Once?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848262#M4164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already tested flashing two boards simultaneous. Further experiments/testing with OpenSDA and more boards is up to you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Oct 2018 17:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Flash-Multiple-S32K144-Boards-At-Once/m-p/848262#M4164</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-10-02T17:19:26Z</dc:date>
    </item>
  </channel>
</rss>