<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studioのトピックs32 dessign studio SDK multicore project</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/s32-dessign-studio-SDK-multicore-project/m-p/846151#M4123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;BR /&gt;I am creating a project to run on multiple cores. Just for testing whether all the cores run in parallel I configured 3 user LEDs(one for each core) to blink continuously. First when i run program for coreZ4_0 and then when I run program for coreZ4_1, the LED configured for coreZ4_0 stops blinking. The same happens for CoreZ2. But only that after I run program for coreZ2, LED configured for CoreZ4_1 does not stop blinking. i.e. CoreZ4_1 and CoreZ2 can run parallel.&lt;BR /&gt;What might be the reason for the core getting blocked?&amp;nbsp;Are there any&amp;nbsp;additional settings that should be done?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jan 2019 05:25:15 GMT</pubDate>
    <dc:creator>kpdeshpande08</dc:creator>
    <dc:date>2019-01-02T05:25:15Z</dc:date>
    <item>
      <title>s32 dessign studio SDK multicore project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32-dessign-studio-SDK-multicore-project/m-p/846151#M4123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;BR /&gt;I am creating a project to run on multiple cores. Just for testing whether all the cores run in parallel I configured 3 user LEDs(one for each core) to blink continuously. First when i run program for coreZ4_0 and then when I run program for coreZ4_1, the LED configured for coreZ4_0 stops blinking. The same happens for CoreZ2. But only that after I run program for coreZ2, LED configured for CoreZ4_1 does not stop blinking. i.e. CoreZ4_1 and CoreZ2 can run parallel.&lt;BR /&gt;What might be the reason for the core getting blocked?&amp;nbsp;Are there any&amp;nbsp;additional settings that should be done?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 05:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32-dessign-studio-SDK-multicore-project/m-p/846151#M4123</guid>
      <dc:creator>kpdeshpande08</dc:creator>
      <dc:date>2019-01-02T05:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: s32 dessign studio SDK multicore project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/s32-dessign-studio-SDK-multicore-project/m-p/846152#M4124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the scenario but I was not able to reproduce it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide more details regarding SDK version, board and CPU used?&lt;/P&gt;&lt;P&gt;Can you share a small application which I can use to reproduce your actual code sequence?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Rares&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 15:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/s32-dessign-studio-SDK-multicore-project/m-p/846152#M4124</guid>
      <dc:creator>raresvasile</dc:creator>
      <dc:date>2019-01-07T15:09:22Z</dc:date>
    </item>
  </channel>
</rss>