<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32DS Project with MAC57D5xx, A5 project not able to start</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Project-with-MAC57D5xx-A5-project-not-able-to-start/m-p/532691#M404</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello nitin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is caused by the fact A5 core is not active when you debug it. The only active core after reset is M4 which setups the other cores to run.&lt;/P&gt;&lt;P&gt;Therefore I'd suggest you to debug entire multicore project by selecting an appropriate Launch Group configuration instead of a separate GDB PEmicro configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;The A5 adn M0 cores are already running when M4 stops at main() - this might be confusing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/936i3B36FFC82C018054/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Aug 2016 15:26:58 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2016-08-01T15:26:58Z</dc:date>
    <item>
      <title>S32DS Project with MAC57D5xx, A5 project not able to start</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Project-with-MAC57D5xx-A5-project-not-able-to-start/m-p/532690#M403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I have a MAC57D54H board with PE Micro debugger connected to it.&lt;/P&gt;&lt;P&gt;I Create a new S32DS Project choosing Family MAC57D5xx with all the toolchain selected, M4, A5 and M0+. &lt;/P&gt;&lt;P&gt;Three projects are created and I select and build the A5 project; then click on debug (choosing Debug Debug_RAM or release, any of the options).&lt;/P&gt;&lt;P&gt;Debug progress gets stuck at 90% (message says "configuring GDB") and after waiting for sometime I get a message &lt;/P&gt;&lt;P&gt;"Launching NXM_XXXXX_A5_Debug_RAM has encountered a problem" and in the details Section it is written as follows:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error in final launch sequence&lt;/P&gt;&lt;P&gt;Failed to execute MI command:&lt;/P&gt;&lt;P&gt;-target-select remote localhost:7226&lt;/P&gt;&lt;P&gt;Error message from debugger back end:&lt;/P&gt;&lt;P&gt;localhost:7226: The system tried to join a drive to a directory on a joined drive.&lt;/P&gt;&lt;P&gt;localhost:7226: The system tried to join a drive to a directory on a joined drive.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I created this project with default settings and have PE Micro as the debugger connected to the PC and the board. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Whereas If I choose M4 project it debugs and runs without any error.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any Idea what is the issue or how I can make A5 run on this board with default project?&lt;/P&gt;&lt;P&gt;My main intention is to run both A5 and M4 on the board.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;nitin &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jul 2016 05:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Project-with-MAC57D5xx-A5-project-not-able-to-start/m-p/532690#M403</guid>
      <dc:creator>nitindhingra</dc:creator>
      <dc:date>2016-07-25T05:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS Project with MAC57D5xx, A5 project not able to start</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Project-with-MAC57D5xx-A5-project-not-able-to-start/m-p/532691#M404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello nitin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is caused by the fact A5 core is not active when you debug it. The only active core after reset is M4 which setups the other cores to run.&lt;/P&gt;&lt;P&gt;Therefore I'd suggest you to debug entire multicore project by selecting an appropriate Launch Group configuration instead of a separate GDB PEmicro configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;The A5 adn M0 cores are already running when M4 stops at main() - this might be confusing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/936i3B36FFC82C018054/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2016 15:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-Project-with-MAC57D5xx-A5-project-not-able-to-start/m-p/532691#M404</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2016-08-01T15:26:58Z</dc:date>
    </item>
  </channel>
</rss>