<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FlexTimer_ic Error Handling in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/FlexTimer-ic-Error-Handling/m-p/835511#M3973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm uisng FlexTimer_ic (using FTM2) to capture two signals phase shifted using Ch0 and Ch2&lt;BR /&gt;interrupt of Ch0 must be fired when detecting rising of the first signal and interrupt of Ch2 must be fired whend detecting Falling edge of the second signal.&lt;/P&gt;&lt;P&gt;However, sometimes the interrupt of Ch2 is triggired with the interrupt of Ch0 and without having a falling edge on Ch2. To clarify this please check the image below:&lt;BR /&gt;The blue line is the input signal to Ch0.&lt;BR /&gt;The green line is the input signal to Ch2.&lt;/P&gt;&lt;P&gt;The yellow line is set to 0 when the interrupt of Ch2 is triggerd.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71036iE9D69D158D669969/image-size/large?v=v2&amp;amp;px=999" title="scope_10.png" alt="scope_10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see the interrupt of Ch2 is triggered with the rising edge of Ch0.&lt;/P&gt;&lt;P&gt;After some investigations, I suspect being affected by the "ERRATA_E9005".&lt;BR /&gt;ERRATA_E9005: Core: Store immediate overlapping exception return operation might vector to incorrect interrupt.&lt;/P&gt;&lt;P&gt;I'm using GCC v.6.3.1 20170509&lt;/P&gt;&lt;P&gt;Does anyone know a work around or how to fix this issue ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Dec 2018 12:31:18 GMT</pubDate>
    <dc:creator>omneia_elshaer</dc:creator>
    <dc:date>2018-12-27T12:31:18Z</dc:date>
    <item>
      <title>FlexTimer_ic Error Handling</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/FlexTimer-ic-Error-Handling/m-p/835511#M3973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm uisng FlexTimer_ic (using FTM2) to capture two signals phase shifted using Ch0 and Ch2&lt;BR /&gt;interrupt of Ch0 must be fired when detecting rising of the first signal and interrupt of Ch2 must be fired whend detecting Falling edge of the second signal.&lt;/P&gt;&lt;P&gt;However, sometimes the interrupt of Ch2 is triggired with the interrupt of Ch0 and without having a falling edge on Ch2. To clarify this please check the image below:&lt;BR /&gt;The blue line is the input signal to Ch0.&lt;BR /&gt;The green line is the input signal to Ch2.&lt;/P&gt;&lt;P&gt;The yellow line is set to 0 when the interrupt of Ch2 is triggerd.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/71036iE9D69D158D669969/image-size/large?v=v2&amp;amp;px=999" title="scope_10.png" alt="scope_10.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As you can see the interrupt of Ch2 is triggered with the rising edge of Ch0.&lt;/P&gt;&lt;P&gt;After some investigations, I suspect being affected by the "ERRATA_E9005".&lt;BR /&gt;ERRATA_E9005: Core: Store immediate overlapping exception return operation might vector to incorrect interrupt.&lt;/P&gt;&lt;P&gt;I'm using GCC v.6.3.1 20170509&lt;/P&gt;&lt;P&gt;Does anyone know a work around or how to fix this issue ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2018 12:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/FlexTimer-ic-Error-Handling/m-p/835511#M3973</guid>
      <dc:creator>omneia_elshaer</dc:creator>
      <dc:date>2018-12-27T12:31:18Z</dc:date>
    </item>
  </channel>
</rss>