<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックHow to measure the system clock?</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825780#M3858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First explain that the chip I used is S32R274,the IDE is S32 Design Studio for Power 2017 R1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the system clock at 120MHz,and try two ways,one is open the PLL1 fraction function,another is closed.At two situation,I use the I/O toggle to test,find the speed of toggling is equal.And then I set the system clock to be 60MHz,the speed of toggling is a half.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To get the real number of the system clock,I try to read the CMU register,because it has a function for metering the frequence,but just for the IRC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So!!! How can I get the real system clock?Read the register or use the oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 08:03:18 GMT</pubDate>
    <dc:creator>578294688</dc:creator>
    <dc:date>2018-07-18T08:03:18Z</dc:date>
    <item>
      <title>How to measure the system clock?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825780#M3858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First explain that the chip I used is S32R274,the IDE is S32 Design Studio for Power 2017 R1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the system clock at 120MHz,and try two ways,one is open the PLL1 fraction function,another is closed.At two situation,I use the I/O toggle to test,find the speed of toggling is equal.And then I set the system clock to be 60MHz,the speed of toggling is a half.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To get the real number of the system clock,I try to read the CMU register,because it has a function for metering the frequence,but just for the IRC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So!!! How can I get the real system clock?Read the register or use the oscilloscope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 08:03:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825780#M3858</guid>
      <dc:creator>578294688</dc:creator>
      <dc:date>2018-07-18T08:03:18Z</dc:date>
    </item>
    <item>
      <title>Re: How to measure the system clock?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825781#M3859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the easiest way is enable clock out and use oscilloscope:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65868iBD70DE4FA8C0CAA4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Jul 2018 09:01:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825781#M3859</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-07-19T09:01:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to measure the system clock?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825782#M3860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,Jiri.&lt;/P&gt;&lt;P&gt;This is a easiest way to solve the problem,it may be that I don't clear my meaning,I just have the daughter board of the EVB board,I can not measure the CLK_OUT pin.Do you have other methods?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 00:51:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-measure-the-system-clock/m-p/825782#M3860</guid>
      <dc:creator>578294688</dc:creator>
      <dc:date>2018-07-20T00:51:43Z</dc:date>
    </item>
  </channel>
</rss>