<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Make Error for CSI source in VSDK_1.1.1 in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Make-Error-for-CSI-source-in-VSDK-1-1-1/m-p/822724#M3799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;EM&gt;make&lt;/EM&gt; for the available library kernel source code like CSI is giving error as below:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79654iC2FDDCDF56CF38B9/image-size/large?v=v2&amp;amp;px=999" title="Error.JPG" alt="Error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What exactly needs to be defined to resolve the above error in the Makefile?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The details for the setup are:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;VSDK:&lt;/STRONG&gt; S32V234 vsdk&amp;nbsp;RTM 1.1.1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Tool:&lt;/STRONG&gt; MSYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Aug 2018 12:20:47 GMT</pubDate>
    <dc:creator>hemansinghtchau</dc:creator>
    <dc:date>2018-08-06T12:20:47Z</dc:date>
    <item>
      <title>Make Error for CSI source in VSDK_1.1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Make-Error-for-CSI-source-in-VSDK-1-1-1/m-p/822724#M3799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The &lt;EM&gt;make&lt;/EM&gt; for the available library kernel source code like CSI is giving error as below:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79654iC2FDDCDF56CF38B9/image-size/large?v=v2&amp;amp;px=999" title="Error.JPG" alt="Error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What exactly needs to be defined to resolve the above error in the Makefile?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The details for the setup are:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;VSDK:&lt;/STRONG&gt; S32V234 vsdk&amp;nbsp;RTM 1.1.1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Tool:&lt;/STRONG&gt; MSYS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 12:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Make-Error-for-CSI-source-in-VSDK-1-1-1/m-p/822724#M3799</guid>
      <dc:creator>hemansinghtchau</dc:creator>
      <dc:date>2018-08-06T12:20:47Z</dc:date>
    </item>
    <item>
      <title>Re: Make Error for CSI source in VSDK_1.1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Make-Error-for-CSI-source-in-VSDK-1-1-1/m-p/822725#M3800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this variable should point into s32v234 kernel sources (more details on VisionSDK_UserGuide.pdf - located in s32v234_sdk/docs/vsdk). Sources are not part of VSDK installation.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway - there are already binary kernel modules present in VSDK. To build them makes sense only if you are doing some changes.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Aug 2018 13:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Make-Error-for-CSI-source-in-VSDK-1-1-1/m-p/822725#M3800</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-08-06T13:06:22Z</dc:date>
    </item>
  </channel>
</rss>