<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I have a problem with NXP AUTOSAR MCAL Software setup in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817171#M3705</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to answer both the issues, in order below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In case of the first image,&lt;/STRONG&gt; it may be possible that you have the MCAL plugins for RTM 1.0.3, but you are trying to import a project created on RTM1.0.4 plugins (or vice-versa). &lt;STRONG&gt;You need to make sure that both MCAL plugins and the tresos workspace project have to the same release version.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The clue is given by: TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;x&lt;/STRONG&gt;R0 'code/id' which has to be consistent both in the names of the plugins (i.e. Mcu_TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0) and XDM files for &lt;EM&gt;&lt;STRONG&gt;workspace\[your_project]\config&lt;/STRONG&gt;&lt;/EM&gt; folder and/or EPC files from &lt;EM&gt;&lt;STRONG&gt;workspace\[your_project]\output\output. &lt;BR /&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Copy the&lt;STRONG&gt; TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;x&lt;/STRONG&gt;R0 &lt;/STRONG&gt;&lt;/EM&gt;id from one of the plugin folders&lt;EM&gt;&lt;STRONG&gt; and do a search for this code in the workspace from where you want to load the configuration. &lt;/STRONG&gt;&lt;/EM&gt;If by any chances these ID's don't match (i.e. you are using RTM1.0.4. plugins with RTM1.0.3 configuration) there are two ways to adapt the 1.0.3 configuration to match the plugins...&lt;/P&gt;&lt;P&gt;- go to each EPC file and change TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;3&lt;/STRONG&gt;R0 to TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0 and do a Import of the new module configuration.(see below)&lt;/P&gt;&lt;P&gt;- or&amp;nbsp; change&amp;nbsp;TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;3&lt;/STRONG&gt;R0 to TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0 in &lt;STRONG&gt;ALL &lt;/STRONG&gt;xdm files... and re-import the entire project (and pray :smileyhappy:&amp;nbsp; because this doesn't always work)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The second issue&lt;/STRONG&gt; is a bit strange...&lt;/P&gt;&lt;P&gt;First make sure that you use the correct Tresos version (24.1.0 or at least 24.0.1). There are some major differences between these Tresos versions regarding AUTOSAR variant handling concept which impacts how configurations are generated/handled by the tool.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Also, make sure that your are not mixing releases.... MCAL MPC574xP configuration will not work with MPC574xG&lt;/P&gt;&lt;P&gt;plugins or vice-versa.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be the case where your tresos project paths get (somehow) mixed and you might not be able to correctly load a project. In that case, the best solution is to create a NEW project from scratch AND import the EPC files for each MCAL module, by using &lt;EM&gt;Import&lt;/EM&gt; option from the project specific &lt;EM&gt;context menu.&lt;/EM&gt; (I attached some pics on how to do all this)&lt;/P&gt;&lt;P&gt;First create new from: main menu&lt;EM&gt;/File/Configuration Project&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NewProject1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78267iDE91E819F1D3DED5/image-size/large?v=v2&amp;amp;px=999" role="button" title="NewProject1.PNG" alt="NewProject1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note. you can provide any name you wish to the project, but I suggest you use one that actually represents the platform and release version you are working with (i.e. MPC574xG_RTM100_asr4.3). Also, AUTOSAR release versions can be &lt;EM&gt;Mixed&lt;/EM&gt; or &lt;EM&gt;4.3.1&lt;/EM&gt; depending on your needs... (for now, you may leave it as ''mixed'')... press next and...&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="newProject2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78305iA0A5945F2B1A5C5D/image-size/large?v=v2&amp;amp;px=999" role="button" title="newProject2.PNG" alt="newProject2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;add platform specific information...&lt;/P&gt;&lt;P&gt;Note. for MCAL configuration Ecu ID in not really important. However, for a series project where other ASR components will be configured, it may be a good idea to have this name consistent with the ecuc name where you will store the entire BSW configuration (though import options should work nevertheless)&lt;/P&gt;&lt;P&gt;Press next (not finish) so you can add which modules you want to use...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="newProject3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78330iD9FAFCF0960FFD50/image-size/large?v=v2&amp;amp;px=999" role="button" title="newProject3.PNG" alt="newProject3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPC574xG ASR4.3 RTM100 release should contain the following modules configured as part of the "sample application" which is, now, called "Integration framework": Adc, Base, Dio, Gpt, Ocu, Mcl, Mcu, Pwm, Port. You need to add all these modules to the configuration and press finish.&lt;/P&gt;&lt;P&gt;Your project should now be created and you should have access to un-configured modules. you need now to import the epc files that where provided for the release by pressing right-mouse-click on the new project to open the context menu import option:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Import.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78395i8D34B43BBA56BFBD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Import.png" alt="Import.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Press the green plus from the next window and this will create an 'importer' for&lt;STRONG&gt; each module...&lt;/STRONG&gt; &lt;span class="lia-inline-image-display-wrapper" image-alt="Adc_import.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78443iF23AE11DE61F34A0/image-size/large?v=v2&amp;amp;px=999" role="button" title="Adc_import.PNG" alt="Adc_import.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pressing &lt;STRONG&gt;Next&lt;/STRONG&gt; will allow you to configure from where to actually import the file. Make sure to use 'Replace' as Import Strategy, to avoid mixing types and also Content type should be: asc:4.3.1 (or what ever ASR release version you are using).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ImportOptions.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78269iCF23D63869C431F7/image-size/large?v=v2&amp;amp;px=999" role="button" title="ImportOptions.PNG" alt="ImportOptions.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Browse to the output folder where the epc files are stored (on your machine), select the corresponding module and press finish.&lt;/P&gt;&lt;P&gt;Press &lt;STRONG&gt;Run Importer &lt;/STRONG&gt;button and you should have an up-to-date ADC configuration... Rinse and repeat for all other modules ... and you should be able to generate the code...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LE.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Final note.&lt;/STRONG&gt; MPC574xG RTM100 AUTOSAR 4.3.1 will only work with Tresos 24.1.0 or newer. Similarly MPC574xG RTM 105 ASR 4.0 will work with tresos 14.x but MAY NOT work with Tresos 24.x.x. Make sure that you use the Tresos version specified in the release notes of the product you are using...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 17:20:59 GMT</pubDate>
    <dc:creator>nxa07100</dc:creator>
    <dc:date>2018-11-28T17:20:59Z</dc:date>
    <item>
      <title>I have a problem with NXP AUTOSAR MCAL Software setup</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817169#M3703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI guys&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had some problem with MCAL Software setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, I watched this page in video&lt;SPAN&gt;(MPC5748G, Tresos Studio 14.1.0, SW574XG-MCAL401-RTMC_&lt;STRONG&gt;SR-1.0.4&lt;/STRONG&gt;)&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;(&lt;A class="link-bare" href="https://www.nxp.com/video/introduction-to-nxp-autosar-mcal-software:AUTOSAR-OnDemand-Training-Video" title="https://www.nxp.com/video/introduction-to-nxp-autosar-mcal-software:AUTOSAR-OnDemand-Training-Video"&gt;https://www.nxp.com/video/introduction-to-nxp-autosar-mcal-software:AUTOSAR-OnDemand-Training-Video&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and I did download MCAL problem in NXP homepage(MPC5748G, Tresos Studio 14.1.0, &lt;STRONG&gt;SW574XG-MCAL401-RTMC_SR-1.0.5&lt;/STRONG&gt;)&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but I had some problem with Load error. blow is that things&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76043i902AF6E47C5E28B5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and I didn't anything so I did download other version MCAL software(&lt;SPAN&gt;Tresos Studio 24.1.0,&amp;nbsp;&lt;STRONG&gt;SW574XG-MCAL431-RTMC_1.0.0&lt;/STRONG&gt;&lt;/SPAN&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so, the load error is fine and we got the Warnings, however, I click the generate file, it has a lot of error. blow is that things&lt;/P&gt;&lt;P&gt;1.warnings file&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_6.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75998i9D8E719CD74520D9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.error file&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_7.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76045iBF6E104ABCCD543D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know how to solve that problems&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;anyone, help to me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best wishs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 09:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817169#M3703</guid>
      <dc:creator>jonghohan</dc:creator>
      <dc:date>2018-10-22T09:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with NXP AUTOSAR MCAL Software setup</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817170#M3704</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you slove the problem? I meet the same problem, I use S32K, and PWM, MCU always report error, I already work on this problem two days, but still report error. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 07:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817170#M3704</guid>
      <dc:creator>cg0</dc:creator>
      <dc:date>2018-11-20T07:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with NXP AUTOSAR MCAL Software setup</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817171#M3705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to answer both the issues, in order below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;In case of the first image,&lt;/STRONG&gt; it may be possible that you have the MCAL plugins for RTM 1.0.3, but you are trying to import a project created on RTM1.0.4 plugins (or vice-versa). &lt;STRONG&gt;You need to make sure that both MCAL plugins and the tresos workspace project have to the same release version.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The clue is given by: TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;x&lt;/STRONG&gt;R0 'code/id' which has to be consistent both in the names of the plugins (i.e. Mcu_TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0) and XDM files for &lt;EM&gt;&lt;STRONG&gt;workspace\[your_project]\config&lt;/STRONG&gt;&lt;/EM&gt; folder and/or EPC files from &lt;EM&gt;&lt;STRONG&gt;workspace\[your_project]\output\output. &lt;BR /&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Copy the&lt;STRONG&gt; TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;x&lt;/STRONG&gt;R0 &lt;/STRONG&gt;&lt;/EM&gt;id from one of the plugin folders&lt;EM&gt;&lt;STRONG&gt; and do a search for this code in the workspace from where you want to load the configuration. &lt;/STRONG&gt;&lt;/EM&gt;If by any chances these ID's don't match (i.e. you are using RTM1.0.4. plugins with RTM1.0.3 configuration) there are two ways to adapt the 1.0.3 configuration to match the plugins...&lt;/P&gt;&lt;P&gt;- go to each EPC file and change TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;3&lt;/STRONG&gt;R0 to TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0 and do a Import of the new module configuration.(see below)&lt;/P&gt;&lt;P&gt;- or&amp;nbsp; change&amp;nbsp;TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;3&lt;/STRONG&gt;R0 to TS_T&lt;STRONG&gt;2&lt;/STRONG&gt;D&lt;STRONG&gt;35&lt;/STRONG&gt;M&lt;STRONG&gt;10&lt;/STRONG&gt;I&lt;STRONG&gt;4&lt;/STRONG&gt;R0 in &lt;STRONG&gt;ALL &lt;/STRONG&gt;xdm files... and re-import the entire project (and pray :smileyhappy:&amp;nbsp; because this doesn't always work)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The second issue&lt;/STRONG&gt; is a bit strange...&lt;/P&gt;&lt;P&gt;First make sure that you use the correct Tresos version (24.1.0 or at least 24.0.1). There are some major differences between these Tresos versions regarding AUTOSAR variant handling concept which impacts how configurations are generated/handled by the tool.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Also, make sure that your are not mixing releases.... MCAL MPC574xP configuration will not work with MPC574xG&lt;/P&gt;&lt;P&gt;plugins or vice-versa.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be the case where your tresos project paths get (somehow) mixed and you might not be able to correctly load a project. In that case, the best solution is to create a NEW project from scratch AND import the EPC files for each MCAL module, by using &lt;EM&gt;Import&lt;/EM&gt; option from the project specific &lt;EM&gt;context menu.&lt;/EM&gt; (I attached some pics on how to do all this)&lt;/P&gt;&lt;P&gt;First create new from: main menu&lt;EM&gt;/File/Configuration Project&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NewProject1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78267iDE91E819F1D3DED5/image-size/large?v=v2&amp;amp;px=999" role="button" title="NewProject1.PNG" alt="NewProject1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note. you can provide any name you wish to the project, but I suggest you use one that actually represents the platform and release version you are working with (i.e. MPC574xG_RTM100_asr4.3). Also, AUTOSAR release versions can be &lt;EM&gt;Mixed&lt;/EM&gt; or &lt;EM&gt;4.3.1&lt;/EM&gt; depending on your needs... (for now, you may leave it as ''mixed'')... press next and...&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="newProject2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78305iA0A5945F2B1A5C5D/image-size/large?v=v2&amp;amp;px=999" role="button" title="newProject2.PNG" alt="newProject2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;add platform specific information...&lt;/P&gt;&lt;P&gt;Note. for MCAL configuration Ecu ID in not really important. However, for a series project where other ASR components will be configured, it may be a good idea to have this name consistent with the ecuc name where you will store the entire BSW configuration (though import options should work nevertheless)&lt;/P&gt;&lt;P&gt;Press next (not finish) so you can add which modules you want to use...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="newProject3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78330iD9FAFCF0960FFD50/image-size/large?v=v2&amp;amp;px=999" role="button" title="newProject3.PNG" alt="newProject3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MPC574xG ASR4.3 RTM100 release should contain the following modules configured as part of the "sample application" which is, now, called "Integration framework": Adc, Base, Dio, Gpt, Ocu, Mcl, Mcu, Pwm, Port. You need to add all these modules to the configuration and press finish.&lt;/P&gt;&lt;P&gt;Your project should now be created and you should have access to un-configured modules. you need now to import the epc files that where provided for the release by pressing right-mouse-click on the new project to open the context menu import option:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Import.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78395i8D34B43BBA56BFBD/image-size/large?v=v2&amp;amp;px=999" role="button" title="Import.png" alt="Import.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Press the green plus from the next window and this will create an 'importer' for&lt;STRONG&gt; each module...&lt;/STRONG&gt; &lt;span class="lia-inline-image-display-wrapper" image-alt="Adc_import.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78443iF23AE11DE61F34A0/image-size/large?v=v2&amp;amp;px=999" role="button" title="Adc_import.PNG" alt="Adc_import.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pressing &lt;STRONG&gt;Next&lt;/STRONG&gt; will allow you to configure from where to actually import the file. Make sure to use 'Replace' as Import Strategy, to avoid mixing types and also Content type should be: asc:4.3.1 (or what ever ASR release version you are using).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ImportOptions.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78269iCF23D63869C431F7/image-size/large?v=v2&amp;amp;px=999" role="button" title="ImportOptions.PNG" alt="ImportOptions.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Browse to the output folder where the epc files are stored (on your machine), select the corresponding module and press finish.&lt;/P&gt;&lt;P&gt;Press &lt;STRONG&gt;Run Importer &lt;/STRONG&gt;button and you should have an up-to-date ADC configuration... Rinse and repeat for all other modules ... and you should be able to generate the code...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LE.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Final note.&lt;/STRONG&gt; MPC574xG RTM100 AUTOSAR 4.3.1 will only work with Tresos 24.1.0 or newer. Similarly MPC574xG RTM 105 ASR 4.0 will work with tresos 14.x but MAY NOT work with Tresos 24.x.x. Make sure that you use the Tresos version specified in the release notes of the product you are using...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 17:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817171#M3705</guid>
      <dc:creator>nxa07100</dc:creator>
      <dc:date>2018-11-28T17:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with NXP AUTOSAR MCAL Software setup</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817172#M3706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alin,&lt;/P&gt;&lt;P&gt;I have the same problem as jongho han. I searched &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;each EPC file to change TS_T&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;2&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;D&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;35&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;M&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;10&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;3&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;R0 but there in every file i found only&amp;nbsp;TS_T&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;2&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;D&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;35&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;M&lt;/SPAN&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;10&lt;/STRONG&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I&lt;STRONG&gt;5&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;R0 which is what i expected as i am using MCAL_1_0_5. I am also using the right version of EB Tresos which is 14.2.1 as specified in the release note of MCAL. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Please help me through this as i havent got any other thread where this problem has been discussed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;Thank you for your valuable time.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Nov 2018 07:58:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817172#M3706</guid>
      <dc:creator>bhavesh</dc:creator>
      <dc:date>2018-11-30T07:58:27Z</dc:date>
    </item>
    <item>
      <title>Re: I have a problem with NXP AUTOSAR MCAL Software setup</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817173#M3707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well that is really strange... if you have the correct plugins it should work...&lt;/P&gt;&lt;P&gt;Please check the following issues:&lt;/P&gt;&lt;P&gt;- go to [tresos_install_directory_root (i.e. c:/tresos)] and check if you have a folder named "links".&lt;/P&gt;&lt;P&gt;- if you have than it should contain one or more *.link files. At least one should be named *MPC574xG_*RTM_1_0_5* or something like that...&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - if there are more than one MPC574xG link files (i.e. one from RTM105 and others from older releases), delete the old versions. Tresos has the issue of getting confused in plugin versions.&lt;/P&gt;&lt;P&gt;- if you have only one link file for MPC574xG open this file for edit and check if the path shown inside it points directly to the folder where you have placed the MCAL plugins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- one last option would be to delete these link files and copy the MCAL plugins together with the *.jar files from the install directory (i.e. c:/NXP/AUTOSAR/[MPC574xG_install_folder]/plugins to [tresos_install_directory_root]/plugins folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Open Tresos again and try to load the project. If this doesn't work it may be something wrong with the licensing and I have no idea how to help there :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&lt;/P&gt;&lt;P&gt;- all the operations described above, should be done while Tresos application is closed.&lt;/P&gt;&lt;P&gt;- make sure that you use either a link file to MPC574xG RTM105 plugins or the the plugins are copied to [tresos_install_directory_root]/plugins folder and NOT BOTH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Dec 2018 11:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/I-have-a-problem-with-NXP-AUTOSAR-MCAL-Software-setup/m-p/817173#M3707</guid>
      <dc:creator>nxa07100</dc:creator>
      <dc:date>2018-12-03T11:02:08Z</dc:date>
    </item>
  </channel>
</rss>