<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: How to change configuration after created a S32DS project</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817153#M3701</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Jiri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;set number additional object files to 0 in 3-cores project, does it means only Z4_0 is active, then Z4_1 and Z2 are disabled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;So I can say that Z4_1 and Z2 are not consuming power?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Jul 2018 05:22:56 GMT</pubDate>
    <dc:creator>barkly_lin</dc:creator>
    <dc:date>2018-07-18T05:22:56Z</dc:date>
    <item>
      <title>How to change configuration after created a S32DS project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817151#M3699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm new guy study S32DS IDE with MPC5748G.&lt;/P&gt;&lt;P&gt;Q1:When I create a new S32DS project, wizard asks me for configuration such as...&lt;/P&gt;&lt;P&gt;1.How many core I need, Boot Z4, Z4, and Z2&lt;/P&gt;&lt;P&gt;2.FLASH Start address and size&lt;/P&gt;&lt;P&gt;3.RAM Start address and size&lt;/P&gt;&lt;P&gt;4.SDKs&lt;/P&gt;&lt;P&gt;After new project created, can I change them?&lt;/P&gt;&lt;P&gt;It seems I have to modify the following files:&lt;/P&gt;&lt;P&gt;\.settings\com.freescale.s32ds.cross.wizard.prefs&lt;/P&gt;&lt;P&gt;flashSize=1d0000&lt;BR /&gt;flashStart=1000000&lt;/P&gt;&lt;P&gt;ramSize=40000&lt;BR /&gt;ramStart=40000000&lt;/P&gt;&lt;P&gt;\Project_Settings\Linker_Files\MPC5748G_flash.ld&lt;/P&gt;&lt;P&gt;flash_rchw : org = 0x00F94000, len = 0x4&lt;BR /&gt; cpu0_reset_vec : org = 0x00F94000+0x10, len = 0x4&lt;BR /&gt; cpu1_reset_vec : org = 0x00F94000+0x14, len = 0x4&lt;BR /&gt; cpu2_reset_vec : org = 0x00F94000+0x04, len = 0x4&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;\Project_Settings\Linker_Files\&lt;/SPAN&gt;MPC5748G_ram.ld&lt;/P&gt;&lt;P&gt;If I disable Z4, Z2 when creating new project, how to enable them and add relative code?&lt;/P&gt;&lt;P&gt;Q2:If I'm not sure which SDKs is required in the future, can I just add them all?&lt;/P&gt;&lt;P&gt;How to make sure I do nothing wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 00:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817151#M3699</guid>
      <dc:creator>barkly_lin</dc:creator>
      <dc:date>2018-07-17T00:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: How to change configuration after created a S32DS project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817152#M3700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;multi-core project technically works as three projects with different linker scripts setup for each core. You can modify linker files later.&amp;nbsp; You should know prior the project creation how many cores you will be using.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have for example three core project - you can remove other core elfs from debug session and use for example only boot Z4_0 core - just set number additional object files to 0&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65635iB8DA170E12FCAA14/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About SDK - good practice is use the last one - ideally RTM version. For MPC5748G is last version v0.9.0 Beta. Unfortunately - EAR and Beta versions are only partly compatible. For SDK change you need to transfer some Processor Expert settings manually.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 08:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817152#M3700</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-07-17T08:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to change configuration after created a S32DS project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817153#M3701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Jiri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;set number additional object files to 0 in 3-cores project, does it means only Z4_0 is active, then Z4_1 and Z2 are disabled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;So I can say that Z4_1 and Z2 are not consuming power?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 05:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-change-configuration-after-created-a-S32DS-project/m-p/817153#M3701</guid>
      <dc:creator>barkly_lin</dc:creator>
      <dc:date>2018-07-18T05:22:56Z</dc:date>
    </item>
  </channel>
</rss>