<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Only CAN_0 in S32DS Debug view</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521156#M358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernhard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the issue and you are correct, there is only CAN_0. It seems it is a bug, so I reported it immediately. Sorry for inconvenience, I hope it will be fix in the next release, which should be available at the end of June.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a workaround, memory view could be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 10:45:10 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2016-06-15T10:45:10Z</dc:date>
    <item>
      <title>Only CAN_0 in S32DS Debug view</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521155#M357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;why is there only CAN_0 in S32_Debug view as seen on the screenshot?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="153614_153614.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/121800i5CF57808FBFA59F4/image-size/large?v=v2&amp;amp;px=999" role="button" title="153614_153614.png" alt="153614_153614.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="CAN.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/59505iAC3CCBA80D8D5284/image-size/large?v=v2&amp;amp;px=999" role="button" title="CAN.png" alt="CAN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using S32DS for PowerPC in verison 1.0 with MPC5748G Eval Board and 176QFP Daughtercard.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 07:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521155#M357</guid>
      <dc:creator>bdn</dc:creator>
      <dc:date>2016-06-15T07:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: Only CAN_0 in S32DS Debug view</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521156#M358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernhard,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the issue and you are correct, there is only CAN_0. It seems it is a bug, so I reported it immediately. Sorry for inconvenience, I hope it will be fix in the next release, which should be available at the end of June.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a workaround, memory view could be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 10:45:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521156#M358</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2016-06-15T10:45:10Z</dc:date>
    </item>
    <item>
      <title>Re: Only CAN_0 in S32DS Debug view</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521157#M359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this issue is _not_ fixed in S32 DS for Power Architecture 1.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 07:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Only-CAN-0-in-S32DS-Debug-view/m-p/521157#M359</guid>
      <dc:creator>bdn</dc:creator>
      <dc:date>2016-06-27T07:22:08Z</dc:date>
    </item>
  </channel>
</rss>