<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: Issue on release mode and not in debug</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805117#M3466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you are creating new project - good idea is add shared Includes/libraries for all configuration together:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63312i2B1B74D7D4956D81/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise you need to add your includes/libs for each configuration manually.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Nov 2018 12:14:00 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2018-11-07T12:14:00Z</dc:date>
    <item>
      <title>Issue on release mode and not in debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805115#M3464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32DS IDE, and I have create a project.&lt;/P&gt;&lt;P&gt;In debug mode I can compile without problem but when I select release mode, the compiler stop due to "fatal error: XXX.h: No such file or directory"&lt;/P&gt;&lt;P&gt;And I saw too, on my workspace, only for release, the folder and files have a square on the left (see picture attached), so nobody knows where come from the problem ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62785iF1EB90A9C77EB1AB/image-size/large?v=v2&amp;amp;px=999" title="IssueRelease.bmp" alt="IssueRelease.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks by advances&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sebastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 12:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805115#M3464</guid>
      <dc:creator>sebastien_ledio</dc:creator>
      <dc:date>2018-11-06T12:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on release mode and not in debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805116#M3465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ok I found myself, in fact in click right on project -&amp;gt; Properties -&amp;gt;C/C++ Build -&amp;gt; Settings -&amp;gt; Standard S32DS C Compiler -&amp;gt; includes, there were not the same includes between debug and release.&lt;/P&gt;&lt;P&gt;So I copied these one of debug to release&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now on debug and release mode, on each folder and file, I have a square on the left, so somebody knows where comes from this issue ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sebastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Nov 2018 13:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805116#M3465</guid>
      <dc:creator>sebastien_ledio</dc:creator>
      <dc:date>2018-11-06T13:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: Issue on release mode and not in debug</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805117#M3466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you are creating new project - good idea is add shared Includes/libraries for all configuration together:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63312i2B1B74D7D4956D81/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise you need to add your includes/libs for each configuration manually.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Nov 2018 12:14:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Issue-on-release-mode-and-not-in-debug/m-p/805117#M3466</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-11-07T12:14:00Z</dc:date>
    </item>
  </channel>
</rss>