<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Change the default compiler version S32DS in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Change-the-default-compiler-version-S32DS/m-p/791322#M3222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S32DS for Vision is supporting gcc 4.9. You can try to add gcc 6.3 by changing some env variables in project properties:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68434i080B904E6170D236/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I'm not sure if it will work. Testing is up to you. gcc 6.3 will be supported with next S32DS Vision release.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Sep 2018 08:48:07 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2018-09-05T08:48:07Z</dc:date>
    <item>
      <title>Change the default compiler version S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Change-the-default-compiler-version-S32DS/m-p/791321#M3221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Change the default compiler version S32DS&lt;BR /&gt;I ran crash on sbc32v234 while compiling the demo project via S32DS.&lt;BR /&gt;I think it should be caused by compiler inconsistency, my hardware bsp17.0 compiler is gcc 6.3.1&lt;BR /&gt;The default compiler for S32DS is gcc 4.9.&lt;BR /&gt;How to change the default compiler?&lt;BR /&gt;Is there a tutorial?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68123iB4B11CC9DFAB7127/image-size/large?v=v2&amp;amp;px=999" title="20180905141646.png" alt="20180905141646.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I changed this and it didn't work. It still crashes when running.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 06:18:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Change-the-default-compiler-version-S32DS/m-p/791321#M3221</guid>
      <dc:creator>435761040</dc:creator>
      <dc:date>2018-09-05T06:18:35Z</dc:date>
    </item>
    <item>
      <title>Re: Change the default compiler version S32DS</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Change-the-default-compiler-version-S32DS/m-p/791322#M3222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;S32DS for Vision is supporting gcc 4.9. You can try to add gcc 6.3 by changing some env variables in project properties:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68434i080B904E6170D236/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I'm not sure if it will work. Testing is up to you. gcc 6.3 will be supported with next S32DS Vision release.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Sep 2018 08:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Change-the-default-compiler-version-S32DS/m-p/791322#M3222</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-09-05T08:48:07Z</dc:date>
    </item>
  </channel>
</rss>