<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32DS EWL and NewLib</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789372#M3185</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the I/O and no I/O means that with I/O you can use printf functionality via Debug probe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The specs option shows which gcc args set was used for library build. You can find these files in S32DS Instalation - [YOUR_INSTALL_PATH]\S32DS_Power_v2017.R1\S32DS\e200_ewl2\lib\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for newlib are .specs located here:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[YOUR_INSTALL_PATH]\&lt;/SPAN&gt;S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\powerpc-eabivle\newlib\lib\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Jul 2018 07:50:02 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2018-07-27T07:50:02Z</dc:date>
    <item>
      <title>S32DS EWL and NewLib</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789371#M3184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I am new to S32DS and have a problem understanding a few parameters regarding the EWL and NewLib libraries for the project.&lt;/P&gt;&lt;P&gt;I have a general idea as to what the libraries are from&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/thread/461435"&gt;S32DS EWL and newlib standard clarification&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1. On creating a new S32R274 Project, under project properties, there following Library supports. What are all these libraries? What id the difference between ewl_c no I/O, &lt;SPAN&gt;ewl_c&amp;nbsp;&lt;/SPAN&gt;Debugger console and &lt;SPAN&gt;ewl_&lt;/SPAN&gt;c9x? How can I know Where can I get information on all the different specs?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66617i8E579F67E7894571/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Su&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 22:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789371#M3184</guid>
      <dc:creator>nxf47968</dc:creator>
      <dc:date>2018-07-26T22:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and NewLib</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789372#M3185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the I/O and no I/O means that with I/O you can use printf functionality via Debug probe.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The specs option shows which gcc args set was used for library build. You can find these files in S32DS Instalation - [YOUR_INSTALL_PATH]\S32DS_Power_v2017.R1\S32DS\e200_ewl2\lib\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for newlib are .specs located here:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[YOUR_INSTALL_PATH]\&lt;/SPAN&gt;S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\powerpc-eabivle\newlib\lib\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 07:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789372#M3185</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-07-27T07:50:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and NewLib</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789373#M3186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jiri,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am trying to create a c++ project under S32DS for KEA128 Controller with newLib_nano no IO. But when i build the project (empty, just main) the code size is about 47k? did i miss anything to set? i did the same with a C Project and the code size is less than 1k?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;another question: if i do not want to use any printf, strings or any library functions, can i set the library support option to none? if i do this i get many linker errors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hani&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 15:56:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-NewLib/m-p/789373#M3186</guid>
      <dc:creator>hanisamara</dc:creator>
      <dc:date>2019-01-02T15:56:20Z</dc:date>
    </item>
  </channel>
</rss>