<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Makefile for My project in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Makefile-for-My-project/m-p/780403#M3045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using s32ds v1.2 power pc for my project which is based on mpc5748g. As per requirement , We need to build Project from command line instead of using s32ds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May be with own make file ,How can I build and generate elf file for my project with own make file ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion can be highly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Dec 2017 05:53:48 GMT</pubDate>
    <dc:creator>yalamandadosaky</dc:creator>
    <dc:date>2017-12-12T05:53:48Z</dc:date>
    <item>
      <title>Makefile for My project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Makefile-for-My-project/m-p/780403#M3045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using s32ds v1.2 power pc for my project which is based on mpc5748g. As per requirement , We need to build Project from command line instead of using s32ds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May be with own make file ,How can I build and generate elf file for my project with own make file ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion can be highly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 05:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Makefile-for-My-project/m-p/780403#M3045</guid>
      <dc:creator>yalamandadosaky</dc:creator>
      <dc:date>2017-12-12T05:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: Makefile for My project</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Makefile-for-My-project/m-p/780404#M3046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can of course create your own makefile and call the command line gcc/binutils yourself:&lt;/P&gt;&lt;P&gt;"c:\NXP\S32DS_Power_v2017.R1\Cross_Tools\powerpc-eabivle-4_9\bin\*"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact IDE project generates make files automatically. So you can adjust the generated makefile to match your need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Other approach is to run eclipse in headless mode and benefit from eclipse IDE features such as makefile generator.&lt;/P&gt;&lt;P&gt;See more info e.g. here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-335704"&gt;HOWTO: S32 Design Studio Command Line Interface&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2014/09/12/building-projects-with-eclipse-from-the-command-line/" title="https://mcuoneclipse.com/2014/09/12/building-projects-with-eclipse-from-the-command-line/"&gt;Building Projects with Eclipse from the Command Line | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 14:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Makefile-for-My-project/m-p/780404#M3046</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-12-12T14:07:19Z</dc:date>
    </item>
  </channel>
</rss>