<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: Debugging an application in S32 IDE not working as expected</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778730#M3020</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-335361"&gt;https://community.nxp.com/docs/DOC-335361&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Feb 2018 11:34:20 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2018-02-02T11:34:20Z</dc:date>
    <item>
      <title>Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778727#M3017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have started debugging an application in S32 IDE, After getting stop in main function, When I do step in, It directly jumps to some task even without initializing &amp;amp; starting OS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is the code which I am trying to debug. When i start debugging, Breakpoints hits the main function &amp;amp; on very next step in, instead of going function CPU_IntDis(), It directly hits the some task. Which I think should only be started when scheduler will schedule it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void) {&lt;BR /&gt; OS_ERR osErr;&lt;BR /&gt; ERR_E err;&lt;/P&gt;&lt;P&gt;//disable all interrupts&lt;BR /&gt; CPU_IntDis();&lt;/P&gt;&lt;P&gt;INIT_sysClk(&amp;amp;err);&lt;BR /&gt; if (err != ERR_OK) {&lt;BR /&gt; while(TRUE);&lt;BR /&gt; }&lt;BR /&gt; OSInit(&amp;amp;osErr);&lt;BR /&gt; SCHTask_init();&lt;BR /&gt; OSStart(&amp;amp;osErr);&lt;/P&gt;&lt;P&gt;while(TRUE);&lt;BR /&gt; return 0;&lt;BR /&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 09:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778727#M3017</guid>
      <dc:creator>p070042</dc:creator>
      <dc:date>2018-02-02T09:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778728#M3018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is your MCU and which version of S32DS are&amp;nbsp;you using?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 09:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778728#M3018</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-02-02T09:53:07Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778729#M3019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I am using MPC5744 &amp;amp; Version of S32 DS is 1.2&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 10:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778729#M3019</guid>
      <dc:creator>p070042</dc:creator>
      <dc:date>2018-02-02T10:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778730#M3020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Isn't your project created for older S32DS version (v1.1)? In v1.2 are changes in linker file and you need perform linker file update. Here are details:&amp;nbsp;&lt;A href="https://community.nxp.com/docs/DOC-335361"&gt;https://community.nxp.com/docs/DOC-335361&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 11:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778730#M3020</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-02-02T11:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778731#M3021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, You are absolutely right, The actual project was created for older version v1.1 and I have imported it in V1.2 and tried to debug it. Yes, this can be the issue.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 11:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778731#M3021</guid>
      <dc:creator>p070042</dc:creator>
      <dc:date>2018-02-02T11:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging an application in S32 IDE not working as expected</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778732#M3022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Thanks very much. Really cool :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;P&gt;It solved my issue.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2018 13:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Debugging-an-application-in-S32-IDE-not-working-as-expected/m-p/778732#M3022</guid>
      <dc:creator>p070042</dc:creator>
      <dc:date>2018-02-02T13:15:52Z</dc:date>
    </item>
  </channel>
</rss>