<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studioのトピックwhat is the difference of debug_flash and debug_ram?</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778685#M3014</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the S32 design studio for ARM R1.&amp;nbsp; I import the example of lptmr_periodic_interrupt_s32k144.&lt;/P&gt;&lt;P&gt;It&amp;nbsp;is running ok in the mode of debug_ram,but it is not ok in the mode of debug_flash. I believe the program reset all the time. Should I set some parameters for debug_flash?&lt;/P&gt;&lt;P&gt;Please help me. Thanks a lot.#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 May 2018 10:25:01 GMT</pubDate>
    <dc:creator>guanyu</dc:creator>
    <dc:date>2018-05-23T10:25:01Z</dc:date>
    <item>
      <title>what is the difference of debug_flash and debug_ram?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778685#M3014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the S32 design studio for ARM R1.&amp;nbsp; I import the example of lptmr_periodic_interrupt_s32k144.&lt;/P&gt;&lt;P&gt;It&amp;nbsp;is running ok in the mode of debug_ram,but it is not ok in the mode of debug_flash. I believe the program reset all the time. Should I set some parameters for debug_flash?&lt;/P&gt;&lt;P&gt;Please help me. Thanks a lot.#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 May 2018 10:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778685#M3014</guid>
      <dc:creator>guanyu</dc:creator>
      <dc:date>2018-05-23T10:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: what is the difference of debug_flash and debug_ram?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778686#M3015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;debug_flash runs program from flash memory (512kB) , debug_ram runs it from MCU's RAM (64kB). There is no special settings. I tried the example - and for me are working both targets (RAM/Flash) without any issue. You can attach project from your workspace - I'll&amp;nbsp; look at it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 May 2018 12:24:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778686#M3015</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-05-23T12:24:48Z</dc:date>
    </item>
    <item>
      <title>Re: what is the difference of debug_flash and debug_ram?</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778687#M3016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess there are two advantages of using debug_ram:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Faster lunch (no need to erase/program flash).&lt;/LI&gt;&lt;LI&gt;Theoretically, no limit on number of breakpoints.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;So, if you have enough ram, use (at&amp;nbsp;early debug phase)&amp;nbsp;debug_ram to verify the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 21:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/what-is-the-difference-of-debug-flash-and-debug-ram/m-p/778687#M3016</guid>
      <dc:creator>MPC8313ERDB_h</dc:creator>
      <dc:date>2018-05-24T21:30:30Z</dc:date>
    </item>
  </channel>
</rss>