<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: Assembly error</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Assembly-error/m-p/775491#M2962</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are probably trying to migrate a project from CodeWarrior into S32DS for Power (GCC).&lt;/P&gt;&lt;P&gt;Function level in line assembly is a feature specific to CodeWarrior project and cannot be migrated as-is into S32DS.&lt;/P&gt;&lt;P&gt;You can either create an asm function in .s file or "C" function with inline __asm(" ") statements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you to create a new project using S32DS New project Wizard for your device. It also includes the interrupt controller initialization so you might use new project as a template.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Dec 2017 08:55:52 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2017-12-08T08:55:52Z</dc:date>
    <item>
      <title>Assembly error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Assembly-error/m-p/775490#M2961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two lines in S32DS Power Project,&lt;/P&gt;&lt;P&gt;__asm void EXCEP_InitExceptionHandlers(void);&lt;/P&gt;&lt;P&gt;__asm void INTC_InitINTCInterrupts(void);&lt;/P&gt;&lt;P&gt;Build the project notice me:expected'(' before 'void',&lt;/P&gt;&lt;P&gt;What's wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Dec 2017 07:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Assembly-error/m-p/775490#M2961</guid>
      <dc:creator>qiminggong</dc:creator>
      <dc:date>2017-12-08T07:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: Assembly error</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Assembly-error/m-p/775491#M2962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are probably trying to migrate a project from CodeWarrior into S32DS for Power (GCC).&lt;/P&gt;&lt;P&gt;Function level in line assembly is a feature specific to CodeWarrior project and cannot be migrated as-is into S32DS.&lt;/P&gt;&lt;P&gt;You can either create an asm function in .s file or "C" function with inline __asm(" ") statements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd recommend you to create a new project using S32DS New project Wizard for your device. It also includes the interrupt controller initialization so you might use new project as a template.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Dec 2017 08:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Assembly-error/m-p/775491#M2962</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-12-08T08:55:52Z</dc:date>
    </item>
  </channel>
</rss>