<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Regarding Export the SDK Example code to IAR EWARM in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Regarding-Export-the-SDK-Example-code-to-IAR-EWARM/m-p/766707#M2849</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can export the project file without SDK v0.8.6 to IAR EWARM, but I couldn't export SDK example project file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could guide about it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32 DS 2018 R1, and IAR EWARM v8.22.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Kate Lee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Apr 2018 05:01:57 GMT</pubDate>
    <dc:creator>leekate-b45752</dc:creator>
    <dc:date>2018-04-05T05:01:57Z</dc:date>
    <item>
      <title>Regarding Export the SDK Example code to IAR EWARM</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Regarding-Export-the-SDK-Example-code-to-IAR-EWARM/m-p/766707#M2849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can export the project file without SDK v0.8.6 to IAR EWARM, but I couldn't export SDK example project file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could guide about it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using S32 DS 2018 R1, and IAR EWARM v8.22.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Kate Lee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2018 05:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Regarding-Export-the-SDK-Example-code-to-IAR-EWARM/m-p/766707#M2849</guid>
      <dc:creator>leekate-b45752</dc:creator>
      <dc:date>2018-04-05T05:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding Export the SDK Example code to IAR EWARM</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Regarding-Export-the-SDK-Example-code-to-IAR-EWARM/m-p/766708#M2850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kate,&lt;/P&gt;&lt;P&gt;Which specific example do you mean?&lt;/P&gt;&lt;P&gt;AFAIK the most examples are available only for Standard s32DS GCC toolchain.&lt;/P&gt;&lt;P&gt;Anyway there is one example - Hello World for IAR EWARM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8091i68B375F9DC279B0D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This one you can directly open in IAR EWARM (see below).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8131iF4232EE63262A2E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps...&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 21:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Regarding-Export-the-SDK-Example-code-to-IAR-EWARM/m-p/766708#M2850</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2018-04-11T21:57:25Z</dc:date>
    </item>
  </channel>
</rss>