<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックP.expert not compiling ITOA</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/P-expert-not-compiling-ITOA/m-p/763180#M2786</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'm working with CAN and Uart here, I have 2 projects:&lt;/P&gt;&lt;P&gt;1) project created from examples that is the flexcan_encrypted_s32k144 and,&lt;/P&gt;&lt;P&gt;2) A custom project created with Processor expert added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="text-decoration: underline;"&gt;&lt;STRONG&gt;Note&lt;/STRONG&gt;&lt;/EM&gt;: 1) Both of the projects have EAR SDK 0.8.6 SDKs against which they are being compiled.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 2) Same chunk of code is working fine in the flexcan_encryp example based project but the same is NOT WORKING on custom project with added PE&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 3) ITOA is not getting compiled (says "undefined reference to ITOA"!!)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 4) All the components are configured correctly, interrupts, clocks, can controllers, lpuart etc (even I copied and "generated code" all times!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;When the same SDK is being with same setup and same code used why am I getting all these differences in&amp;nbsp; execution!?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Mar 2018 07:12:25 GMT</pubDate>
    <dc:creator>nishantsood</dc:creator>
    <dc:date>2018-03-16T07:12:25Z</dc:date>
    <item>
      <title>P.expert not compiling ITOA</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/P-expert-not-compiling-ITOA/m-p/763180#M2786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'm working with CAN and Uart here, I have 2 projects:&lt;/P&gt;&lt;P&gt;1) project created from examples that is the flexcan_encrypted_s32k144 and,&lt;/P&gt;&lt;P&gt;2) A custom project created with Processor expert added.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="text-decoration: underline;"&gt;&lt;STRONG&gt;Note&lt;/STRONG&gt;&lt;/EM&gt;: 1) Both of the projects have EAR SDK 0.8.6 SDKs against which they are being compiled.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 2) Same chunk of code is working fine in the flexcan_encryp example based project but the same is NOT WORKING on custom project with added PE&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 3) ITOA is not getting compiled (says "undefined reference to ITOA"!!)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 4) All the components are configured correctly, interrupts, clocks, can controllers, lpuart etc (even I copied and "generated code" all times!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;When the same SDK is being with same setup and same code used why am I getting all these differences in&amp;nbsp; execution!?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 07:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/P-expert-not-compiling-ITOA/m-p/763180#M2786</guid>
      <dc:creator>nishantsood</dc:creator>
      <dc:date>2018-03-16T07:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: P.expert not compiling ITOA</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/P-expert-not-compiling-ITOA/m-p/763181#M2787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EWL library, which is by default used in the projects does not support this function. You must switch your project into NewLib. Please check the figure below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35670i138FD81F45A77D17/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 13:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/P-expert-not-compiling-ITOA/m-p/763181#M2787</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2018-03-20T13:03:44Z</dc:date>
    </item>
  </channel>
</rss>