<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/When-I-try-to-use-the-opencv-s-highgui-to-show-a-frame-there-is/m-p/747203#M2564</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The function is not implemented. Rebuild the library with Windows, GTK+ 2.x or Carbon support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1: is the S32 Design Vision Studio's ocv library compiled with GTK2.0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2: How to compile the GTK for s32v234 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 3: How to compile OpenCV With GTK2.0 for Arm or with QT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2018 13:23:11 GMT</pubDate>
    <dc:creator>justforfunl</dc:creator>
    <dc:date>2018-03-29T13:23:11Z</dc:date>
    <item>
      <title>When I try to use the opencv's highgui to show a frame, there is some error, can not find gtk support</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/When-I-try-to-use-the-opencv-s-highgui-to-show-a-frame-there-is/m-p/747203#M2564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The function is not implemented. Rebuild the library with Windows, GTK+ 2.x or Carbon support. If you are on Ubuntu or Debian, install libgtk2.0-dev and pkg-config, then re-run cmake or configure script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1: is the S32 Design Vision Studio's ocv library compiled with GTK2.0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2: How to compile the GTK for s32v234 kernel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 3: How to compile OpenCV With GTK2.0 for Arm or with QT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 13:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/When-I-try-to-use-the-opencv-s-highgui-to-show-a-frame-there-is/m-p/747203#M2564</guid>
      <dc:creator>justforfunl</dc:creator>
      <dc:date>2018-03-29T13:23:11Z</dc:date>
    </item>
  </channel>
</rss>