<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 and MPC574XG-MB in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32-and-MPC574XG-MB/m-p/743718#M2502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to&amp;nbsp;run/debug the example projects in S32 Design Studio for Power Architecture.&lt;/P&gt;&lt;P&gt;Each project I try to run, keeps giving me the same message "No Source available for "0x1000000".&lt;/P&gt;&lt;P&gt;The debugger looks like it is connecting correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried both "DEBUG RAM" and DEBUG FLASH" to no avail.&lt;/P&gt;&lt;P&gt;I don't know if the projects are specifically for the DEV_KIT board and won't run on the MPC574XG-MB unless I change something?&lt;/P&gt;&lt;P&gt;The daughter card is MPC574XG-176DS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1&lt;BR /&gt;Copyright 2017 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -Ô&lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&amp;amp;E\nxp_mpc5748g_1x32x1520k_cflash.pcp&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Initialized.&lt;BR /&gt; &lt;BR /&gt;;version 1.05, 06/26/2017, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [5748G_6080k]&lt;BR /&gt; &lt;BR /&gt;;device NXP, MPC5748G, 1x32x1520k, desc=CFlash&lt;BR /&gt; &lt;BR /&gt;;begin_cs device=$00F90000, length=$005F0000, ram=$40000000&lt;BR /&gt; &lt;BR /&gt;Loading programming algorithm ... &lt;BR /&gt; &lt;BR /&gt;WARNING - Selected .PCP file has been modified. CRC16 = $5A63 &lt;BR /&gt;Done.&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ... &lt;BR /&gt; block 00FA0000-00FA0003 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 00FA0010-00FA0013 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01000000-01000129 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01001000-010010F3 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01002000-01002C0B ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01002C10-01011DA7 ... &lt;BR /&gt;Ok. &lt;BR /&gt; Checksum Verification Successful. (Cumulative CRC-16=$B0C1) &lt;BR /&gt;Application verified in memory. No need to reprogram. &lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;Debugger retrying force to background mode. &lt;BR /&gt; &lt;BR /&gt;PE-ERROR: Warning. Can't read registers while part is running.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jan 2018 16:19:13 GMT</pubDate>
    <dc:creator>cholland</dc:creator>
    <dc:date>2018-01-22T16:19:13Z</dc:date>
    <item>
      <title>S32 and MPC574XG-MB</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32-and-MPC574XG-MB/m-p/743718#M2502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to&amp;nbsp;run/debug the example projects in S32 Design Studio for Power Architecture.&lt;/P&gt;&lt;P&gt;Each project I try to run, keeps giving me the same message "No Source available for "0x1000000".&lt;/P&gt;&lt;P&gt;The debugger looks like it is connecting correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried both "DEBUG RAM" and DEBUG FLASH" to no avail.&lt;/P&gt;&lt;P&gt;I don't know if the projects are specifically for the DEV_KIT board and won't run on the MPC574XG-MB unless I change something?&lt;/P&gt;&lt;P&gt;The daughter card is MPC574XG-176DS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connection from "127.0.0.1" via 127.0.0.1&lt;BR /&gt;Copyright 2017 P&amp;amp;E Microcomputer Systems,Inc.&lt;BR /&gt;Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -Ô&lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;CMD&amp;gt;CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&amp;amp;E\nxp_mpc5748g_1x32x1520k_cflash.pcp&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Initialized.&lt;BR /&gt; &lt;BR /&gt;;version 1.05, 06/26/2017, Copyright P&amp;amp;E Microcomputer Systems, &lt;A href="https://community.nxp.com/www.pemicro.com" target="test_blank"&gt;www.pemicro.com&lt;/A&gt; [5748G_6080k]&lt;BR /&gt; &lt;BR /&gt;;device NXP, MPC5748G, 1x32x1520k, desc=CFlash&lt;BR /&gt; &lt;BR /&gt;;begin_cs device=$00F90000, length=$005F0000, ram=$40000000&lt;BR /&gt; &lt;BR /&gt;Loading programming algorithm ... &lt;BR /&gt; &lt;BR /&gt;WARNING - Selected .PCP file has been modified. CRC16 = $5A63 &lt;BR /&gt;Done.&lt;BR /&gt;CMD&amp;gt;VC&lt;BR /&gt;Verifying object file CRC-16 to device ranges ... &lt;BR /&gt; block 00FA0000-00FA0003 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 00FA0010-00FA0013 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01000000-01000129 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01001000-010010F3 ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01002000-01002C0B ... &lt;BR /&gt;Ok. &lt;BR /&gt; block 01002C10-01011DA7 ... &lt;BR /&gt;Ok. &lt;BR /&gt; Checksum Verification Successful. (Cumulative CRC-16=$B0C1) &lt;BR /&gt;Application verified in memory. No need to reprogram. &lt;BR /&gt; &lt;BR /&gt;CMD&amp;gt;RE&lt;BR /&gt; &lt;BR /&gt;Initializing.&lt;BR /&gt;MPC574xB/C/D Device detected. &lt;BR /&gt;Target has been RESET and is active.&lt;BR /&gt;Debugger retrying force to background mode. &lt;BR /&gt; &lt;BR /&gt;PE-ERROR: Warning. Can't read registers while part is running.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 16:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32-and-MPC574XG-MB/m-p/743718#M2502</guid>
      <dc:creator>cholland</dc:creator>
      <dc:date>2018-01-22T16:19:13Z</dc:date>
    </item>
  </channel>
</rss>