<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックSA support in VSDK1.1</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716346#M2015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the release notes i see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;BR /&gt;ISP&lt;BR /&gt; o AVB Video Listener updates integration.&lt;BR /&gt; o &lt;STRONG&gt;Bare-metal support excluded.&lt;/STRONG&gt;&lt;BR /&gt; o CGD&lt;BR /&gt; o I2C API updated. Added support for 16bit register accesses.&lt;BR /&gt; o CGD support for MA2926B/MAX9295A&lt;BR /&gt; o TI Deserializer &amp;amp; AR0140 Camera (ON Semi)&lt;BR /&gt; o Sequencer FW partitioning supporting new static sequencing &lt;BR /&gt; and binary distribution&lt;BR /&gt; o Added a new BSP patch (os/linux/s32v234_dtsi_400kbps_IIC.patch) which&lt;BR /&gt; enables 400 Kbps on IIC. Not used in prebuilt BSP. If 400 Kbps on IIC&lt;BR /&gt; is needed, BSP (Linux) needs to be rebuilt with this patch applied.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does the Bare-metal support exclusion refer to Standalone mode? I cannot find any SA related build directories in "demos" directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Evgeny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 May 2018 19:36:46 GMT</pubDate>
    <dc:creator>evgenyerlihman</dc:creator>
    <dc:date>2018-05-23T19:36:46Z</dc:date>
    <item>
      <title>SA support in VSDK1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716346#M2015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the release notes i see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;&lt;BR /&gt;ISP&lt;BR /&gt; o AVB Video Listener updates integration.&lt;BR /&gt; o &lt;STRONG&gt;Bare-metal support excluded.&lt;/STRONG&gt;&lt;BR /&gt; o CGD&lt;BR /&gt; o I2C API updated. Added support for 16bit register accesses.&lt;BR /&gt; o CGD support for MA2926B/MAX9295A&lt;BR /&gt; o TI Deserializer &amp;amp; AR0140 Camera (ON Semi)&lt;BR /&gt; o Sequencer FW partitioning supporting new static sequencing &lt;BR /&gt; and binary distribution&lt;BR /&gt; o Added a new BSP patch (os/linux/s32v234_dtsi_400kbps_IIC.patch) which&lt;BR /&gt; enables 400 Kbps on IIC. Not used in prebuilt BSP. If 400 Kbps on IIC&lt;BR /&gt; is needed, BSP (Linux) needs to be rebuilt with this patch applied.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Does the Bare-metal support exclusion refer to Standalone mode? I cannot find any SA related build directories in "demos" directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Evgeny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 May 2018 19:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716346#M2015</guid>
      <dc:creator>evgenyerlihman</dc:creator>
      <dc:date>2018-05-23T19:36:46Z</dc:date>
    </item>
    <item>
      <title>Re: SA support in VSDK1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716347#M2016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, support for bare-metal project was removed from VSDK RTM v1.1.0. The reason is that only few customers was using it this way - mostly internally. Vast majority is using Linux on target machine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 09:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716347#M2016</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-05-24T09:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: SA support in VSDK1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716348#M2017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jiri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an easy way for me, given i already have a SA app, to update the sequencer firmware to work in static mode? Using vsdk1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Evgeny&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 13:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716348#M2017</guid>
      <dc:creator>evgenyerlihman</dc:creator>
      <dc:date>2018-05-24T13:20:17Z</dc:date>
    </item>
    <item>
      <title>Re: SA support in VSDK1.1</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716349#M2018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm afraid that there is no easy way. You can try import new source codes in old VSDK and try build it with standalone confuguration. But I didn't check the differences between these two versions. I have only the 1.1 version ritght now.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jiri&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 08:41:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/SA-support-in-VSDK1-1/m-p/716349#M2018</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2018-06-01T08:41:18Z</dc:date>
    </item>
  </channel>
</rss>