<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS EWL and newlib standard clarification in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696808#M1636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dan -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response.&amp;nbsp; We will dig into it some more and will let you know if I find anything useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jan 2018 15:38:56 GMT</pubDate>
    <dc:creator>j_cole</dc:creator>
    <dc:date>2018-01-26T15:38:56Z</dc:date>
    <item>
      <title>S32DS EWL and newlib standard clarification</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696805#M1633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with S32DS for Power Architecture v1.2 for a future medical product. We are trying to decide between selecting EWL or newlib standard C libraries, both of which are bundled with S32DS. According to the bundled documentation, the following versions are installed:&lt;/P&gt;&lt;P&gt;* The Red Hat newlib C Library - libc 2.2.0 - December 2014&lt;/P&gt;&lt;P&gt;* EWL C Reference Manual - Document Number: CWEWLCREF Rev 10.x, 02/2014&lt;/P&gt;&lt;P&gt;* EWL C++ Library Reference - Document Number: CWEWLCPPREF Rev 10.x, 02/2014&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please comment on the following questions?&lt;/P&gt;&lt;P&gt;1. Can you comment on the level of testing performed on EWL and newlib for&amp;nbsp; suitability of their use in medical applications?&lt;/P&gt;&lt;P&gt;2. What is the notification process when NXP releases patches for newlib/stdlibc++?&lt;/P&gt;&lt;P&gt;3. Will both EWL and newlib be maintained going forward or is either being deprecated?&lt;/P&gt;&lt;P&gt;4.a. To which ISO C++ standard does EWL conform to? EWL C++ Library Reference Rev 10.x is very vague on this topic. (More specifically does EWL support modern C++?)&lt;/P&gt;&lt;P&gt;4.b. To which ISO C standard does newlib conform to? I didn't see any reference to anything newer than ISO9899 "C99".&lt;/P&gt;&lt;P&gt;4.c. To which ISO C++ standard does newlib/stdlibc++ conform to?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 20:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696805#M1633</guid>
      <dc:creator>dan_teodorescu</dc:creator>
      <dc:date>2017-10-02T20:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and newlib standard clarification</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696806#M1634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are also in the process of evaluating the two libraries and have similar concerns.&amp;nbsp; Have you found answers to some/all of the questions you are asking?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 17:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696806#M1634</guid>
      <dc:creator>j_cole</dc:creator>
      <dc:date>2018-01-24T17:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and newlib standard clarification</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696807#M1635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't received formal confirmation on this topic. I suspect that EWL was designed per C99 / C++03 standards, and is probably too costly to upgrade to the latest standards. For many projects, the older standards are perfectly acceptable. newlib/stdlibc++ are attractive because they support the newer standards, but NXP will probably provide only limited support as these are community-based projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jan 2018 19:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696807#M1635</guid>
      <dc:creator>dan_teodorescu</dc:creator>
      <dc:date>2018-01-25T19:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and newlib standard clarification</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696808#M1636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dan -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the response.&amp;nbsp; We will dig into it some more and will let you know if I find anything useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 15:38:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696808#M1636</guid>
      <dc:creator>j_cole</dc:creator>
      <dc:date>2018-01-26T15:38:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS EWL and newlib standard clarification</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696809#M1637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure what compiler you are using, but something else to consider is that the&amp;nbsp;GCC compiler&amp;nbsp;is almost completely, but not&amp;nbsp;fully, ISO C99 or ISO C11 compliant.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See&amp;nbsp;&lt;A class="link-titled" href="https://gcc.gnu.org/wiki/C11Status" title="https://gcc.gnu.org/wiki/C11Status"&gt;C11Status - GCC Wiki&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 17:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-EWL-and-newlib-standard-clarification/m-p/696809#M1637</guid>
      <dc:creator>j_cole</dc:creator>
      <dc:date>2018-01-26T17:43:48Z</dc:date>
    </item>
  </channel>
</rss>