<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studioのトピックpowerpc cross-tool chain problem with SCons maker</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/powerpc-cross-tool-chain-problem-with-SCons-maker/m-p/689474#M1533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to write a SCons script to build my project, which was originally built in S32DS.&lt;/P&gt;&lt;P&gt;The project built fine with the Microsoft Visual C++ compiler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, after specify the compiler PATH and the compiler powerpc-eabivle-gcc to use when building the project( that's the only environment setting I changed for the build), I got an error from powerpc-eabivle-gcc for every header file folder I include with CPPPATH, that there is no such file or directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm wondering if there's any special settings I need just for this compiler. Thanks for any suggestions/help:)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ruonan &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Jul 2017 18:44:46 GMT</pubDate>
    <dc:creator>ruonanzhou</dc:creator>
    <dc:date>2017-07-31T18:44:46Z</dc:date>
    <item>
      <title>powerpc cross-tool chain problem with SCons maker</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/powerpc-cross-tool-chain-problem-with-SCons-maker/m-p/689474#M1533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to write a SCons script to build my project, which was originally built in S32DS.&lt;/P&gt;&lt;P&gt;The project built fine with the Microsoft Visual C++ compiler.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, after specify the compiler PATH and the compiler powerpc-eabivle-gcc to use when building the project( that's the only environment setting I changed for the build), I got an error from powerpc-eabivle-gcc for every header file folder I include with CPPPATH, that there is no such file or directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm wondering if there's any special settings I need just for this compiler. Thanks for any suggestions/help:)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ruonan &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 18:44:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/powerpc-cross-tool-chain-problem-with-SCons-maker/m-p/689474#M1533</guid>
      <dc:creator>ruonanzhou</dc:creator>
      <dc:date>2017-07-31T18:44:46Z</dc:date>
    </item>
    <item>
      <title>Re: powerpc cross-tool chain problem with SCons maker</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/powerpc-cross-tool-chain-problem-with-SCons-maker/m-p/689475#M1534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please write more detail ? Especially command line switches and console output.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 19:16:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/powerpc-cross-tool-chain-problem-with-SCons-maker/m-p/689475#M1534</guid>
      <dc:creator>alexanderfedoto</dc:creator>
      <dc:date>2017-08-03T19:16:20Z</dc:date>
    </item>
  </channel>
</rss>