<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design Studio中的主题 Re: S32DS to 5744P errior</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689334#M1519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please provide us with more details about the issue you are facing?&lt;/P&gt;&lt;P&gt;Can you attach screenshot of the download error?&lt;/P&gt;&lt;P&gt;Which demo code are you trying to download? Does it run correctly in the debugger but crashes after POR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a known issue related to RCHW setup if the compiler optimization is set to level 3 (Release Build Configuration). This causes the objects are allocated in reversed order - reset vector is swapped with rchw word and the device does not boot-up after POR. This should be fixed in the next release. I attached fixed file (flashrchw.c).&lt;/P&gt;&lt;P&gt;If this is your case please replace this file in your project and rebuild.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 May 2017 06:45:23 GMT</pubDate>
    <dc:creator>stanish</dc:creator>
    <dc:date>2017-05-23T06:45:23Z</dc:date>
    <item>
      <title>S32DS to 5744P errior</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689333#M1518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I download demo code to 5744P by S32ds ，have an errior，after I power on，the software&amp;nbsp; doesn't run.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 May 2017 03:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689333#M1518</guid>
      <dc:creator>haiyangliu</dc:creator>
      <dc:date>2017-05-23T03:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS to 5744P errior</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689334#M1519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Could you please provide us with more details about the issue you are facing?&lt;/P&gt;&lt;P&gt;Can you attach screenshot of the download error?&lt;/P&gt;&lt;P&gt;Which demo code are you trying to download? Does it run correctly in the debugger but crashes after POR?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a known issue related to RCHW setup if the compiler optimization is set to level 3 (Release Build Configuration). This causes the objects are allocated in reversed order - reset vector is swapped with rchw word and the device does not boot-up after POR. This should be fixed in the next release. I attached fixed file (flashrchw.c).&lt;/P&gt;&lt;P&gt;If this is your case please replace this file in your project and rebuild.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 May 2017 06:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689334#M1519</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-05-23T06:45:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS to 5744P errior</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689335#M1520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I created a project and it works while debuging.But it seems my code did not load in the flash, and if I power on MPC5744 again,the code can't work.While debuging,an error occured as follows.Does it cause the problem? I tried other demos as well, such as PIT demo, the error still occured.&lt;span class="lia-inline-image-display-wrapper" image-alt="VEV~8J][JUAM92{ANSHF2HA.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19916i4F027BD19E031089/image-size/large?v=v2&amp;amp;px=999" role="button" title="VEV~8J][JUAM92{ANSHF2HA.png" alt="VEV~8J][JUAM92{ANSHF2HA.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 May 2017 08:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689335#M1520</guid>
      <dc:creator>haiyangliu</dc:creator>
      <dc:date>2017-05-23T08:01:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS to 5744P errior</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689336#M1521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"No Source available for 0x1000000" may not indicate it's flash programming error.&lt;/P&gt;&lt;P&gt;Can you post the content your GDB server&amp;nbsp;console (I can see snippet of it at bottom right corner of your screenshot).&lt;/P&gt;&lt;P&gt;Are you able to reach main() when the debugger session is established?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Stan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 May 2017 15:48:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32DS-to-5744P-errior/m-p/689336#M1521</guid>
      <dc:creator>stanish</dc:creator>
      <dc:date>2017-05-23T15:48:55Z</dc:date>
    </item>
  </channel>
</rss>