<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックAMMCLib support for S32R294 e200z7 cores</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2406748#M14412</link>
    <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;We are developing an application for the S32R294 and would like to use AMMCLib on its e200z7 cores.&lt;/P&gt;&lt;P&gt;Is there an AMMCLib release that officially supports the S32R294? If not, could you recommend another NXP-provided math library that is compatible with the S32R294 e200z7 core?&lt;/P&gt;&lt;P&gt;Please also let us know whether a specific S32 Design Studio toolchain, SDK, or RSDK version is required.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 20 Aug 2026 02:26:58 GMT</pubDate>
    <dc:creator>CSBoy</dc:creator>
    <dc:date>2026-08-20T02:26:58Z</dc:date>
    <item>
      <title>AMMCLib support for S32R294 e200z7 cores</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2406748#M14412</link>
      <description>&lt;P&gt;Hello NXP team,&lt;/P&gt;&lt;P&gt;We are developing an application for the S32R294 and would like to use AMMCLib on its e200z7 cores.&lt;/P&gt;&lt;P&gt;Is there an AMMCLib release that officially supports the S32R294? If not, could you recommend another NXP-provided math library that is compatible with the S32R294 e200z7 core?&lt;/P&gt;&lt;P&gt;Please also let us know whether a specific S32 Design Studio toolchain, SDK, or RSDK version is required.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Aug 2026 02:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2406748#M14412</guid>
      <dc:creator>CSBoy</dc:creator>
      <dc:date>2026-08-20T02:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: AMMCLib support for S32R294 e200z7 cores</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2406991#M14416</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is not an AMMCLib release that officially supports the S32R294 platform.&lt;/P&gt;
&lt;P&gt;The AMMCLib device support list currently includes several Power Architecture MCU families (for example MPC577xK/MPC5775E), but S32R294 is not listed as a supported target.&lt;/P&gt;
&lt;P&gt;For S32R294 development, NXP's primary software offering is the Radar SDK for S32R29x together with the S32 Design Studio Power Architecture toolchain.&lt;/P&gt;
&lt;P&gt;What should be the target application?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 20 Aug 2026 11:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2406991#M14416</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-08-20T11:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: AMMCLib support for S32R294 e200z7 cores</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2407145#M14419</link>
      <description>&lt;P&gt;Hi Peter,&lt;/P&gt;&lt;P&gt;Thank you for the clarification.&lt;/P&gt;&lt;P&gt;Our target application is a radar signal-processing pipeline. We plan to run the following algorithms on the S32R294 e200z7 cores:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;DML-based direction-of-arrival estimation&lt;/LI&gt;&lt;LI&gt;A small number of FFT operations&lt;/LI&gt;&lt;LI&gt;Kalman filtering, including matrix multiplication, transposition, and linear-system solving or matrix inversion&lt;/LI&gt;&lt;LI&gt;Feature extraction and lightweight radar target classification using vector, matrix, and statistical operations&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Running these algorithms on the e200z7 cores would reduce data transfers and data-format conversions between the SPT and e200z7, which should improve processing efficiency.&lt;/P&gt;&lt;P&gt;We are looking for optimized FFT, complex arithmetic, matrix, vector, and linear algebra functions for the S32R294 e200z7 cores. Does NXP provide a suitable math or DSP library for these use cases?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Fri, 21 Aug 2026 01:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/AMMCLib-support-for-S32R294-e200z7-cores/m-p/2407145#M14419</guid>
      <dc:creator>CSBoy</dc:creator>
      <dc:date>2026-08-21T01:15:45Z</dc:date>
    </item>
  </channel>
</rss>