<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックMissing NXP GCC 10.2 in S32K3 Development Pack for S32 Design Studio 3.6.7 RFP</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/Missing-NXP-GCC-10-2-in-S32K3-Development-Pack-for-S32-Design/m-p/2381098#M14322</link>
    <description>&lt;P&gt;According to the &lt;A href="https://freescaleesd.flexnetoperations.com/337170/541/14064541/SW32K3_S32DS_Development_Pack_3.6.7_RFP_D2604_Release_Notes.pdf?ftpRequestID=4349657161&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20260615034828NDM3NDI3ODYx&amp;amp;authparam=1781520508_3011693faa31d9cf8010bb0af57323e3&amp;amp;ext=.pdf" target="_self"&gt;release note&lt;/A&gt;,&amp;nbsp;the S32K3xx Development Package 3.6.7 RFP contains&amp;nbsp;GCC version&amp;nbsp;11.4, 10.2.0 and 9.4.0.&lt;/P&gt;&lt;P&gt;However, after installation(SW32_S32DS_3.6.7_RFP_D2604_win32.x86_64.exe), there is only&amp;nbsp;GCC version&amp;nbsp;11.4, no 10.2.0 and 9.4.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In S32DS Extensions and Updates, I can also only see GCC 11.4. There are no options for GCC 10.2.0 or GCC 9.4.&lt;/P&gt;&lt;P&gt;My operation system is Windows 10 x64 22H2.&amp;nbsp;I am using an offline computer. I am not sure if that is the cause.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jun 2026 04:18:12 GMT</pubDate>
    <dc:creator>Torris</dc:creator>
    <dc:date>2026-06-15T04:18:12Z</dc:date>
    <item>
      <title>Missing NXP GCC 10.2 in S32K3 Development Pack for S32 Design Studio 3.6.7 RFP</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Missing-NXP-GCC-10-2-in-S32K3-Development-Pack-for-S32-Design/m-p/2381098#M14322</link>
      <description>&lt;P&gt;According to the &lt;A href="https://freescaleesd.flexnetoperations.com/337170/541/14064541/SW32K3_S32DS_Development_Pack_3.6.7_RFP_D2604_Release_Notes.pdf?ftpRequestID=4349657161&amp;amp;server=freescaleesd.flexnetoperations.com&amp;amp;dtm=DTM20260615034828NDM3NDI3ODYx&amp;amp;authparam=1781520508_3011693faa31d9cf8010bb0af57323e3&amp;amp;ext=.pdf" target="_self"&gt;release note&lt;/A&gt;,&amp;nbsp;the S32K3xx Development Package 3.6.7 RFP contains&amp;nbsp;GCC version&amp;nbsp;11.4, 10.2.0 and 9.4.0.&lt;/P&gt;&lt;P&gt;However, after installation(SW32_S32DS_3.6.7_RFP_D2604_win32.x86_64.exe), there is only&amp;nbsp;GCC version&amp;nbsp;11.4, no 10.2.0 and 9.4.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In S32DS Extensions and Updates, I can also only see GCC 11.4. There are no options for GCC 10.2.0 or GCC 9.4.&lt;/P&gt;&lt;P&gt;My operation system is Windows 10 x64 22H2.&amp;nbsp;I am using an offline computer. I am not sure if that is the cause.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 04:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Missing-NXP-GCC-10-2-in-S32K3-Development-Pack-for-S32-Design/m-p/2381098#M14322</guid>
      <dc:creator>Torris</dc:creator>
      <dc:date>2026-06-15T04:18:12Z</dc:date>
    </item>
    <item>
      <title>Re: Missing NXP GCC 10.2 in S32K3 Development Pack for S32 Design Studio 3.6.7 RFP</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/Missing-NXP-GCC-10-2-in-S32K3-Development-Pack-for-S32-Design/m-p/2381205#M14323</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;After installing &lt;STRONG&gt;S32 Design Studio 3.6.7 RFP&lt;/STRONG&gt; on Windows 11, I found that I also needed to select and install "&lt;STRONG&gt;NXP GCC for Arm Embedded Processors v10.2 build 1728&lt;/STRONG&gt;" in &lt;STRONG&gt;S32DS Extensions and Updates&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="NXP GCC for Arm Embedded Processors v10.2 build 1728.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/388974i395D5BBDF9BA1D68/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXP GCC for Arm Embedded Processors v10.2 build 1728.png" alt="NXP GCC for Arm Embedded Processors v10.2 build 1728.png" /&gt;&lt;/span&gt;Sorry for the inconvenience we bring you!&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jun 2026 08:27:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/Missing-NXP-GCC-10-2-in-S32K3-Development-Pack-for-S32-Design/m-p/2381205#M14323</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2026-06-15T08:27:53Z</dc:date>
    </item>
  </channel>
</rss>