<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: ISELED SDK installation issue on S32DS ARM 2018.R1 (Update site not working / Local update fails</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/ISELED-SDK-installation-issue-on-S32DS-ARM-2018-R1-Update-site/m-p/2356942#M14232</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please use S32DS for ARM v2.2 - it is compatible with Iseled v3.9.0&lt;/P&gt;</description>
    <pubDate>Tue, 28 Apr 2026 06:14:16 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2026-04-28T06:14:16Z</dc:date>
    <item>
      <title>ISELED SDK installation issue on S32DS ARM 2018.R1 (Update site not working / Local update fails)</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ISELED-SDK-installation-issue-on-S32DS-ARM-2018-R1-Update-site/m-p/2353410#M14226</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently purchased the ISELED ADK and am currently setting up the development environment.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I am currently setting up the ISELED ADK environment following the official installation guide:&lt;BR /&gt;"NXP_ISELED_SDK Beta 3.9.0 installation guide_09.2019".&lt;/P&gt;&lt;P&gt;I have successfully installed:&lt;BR /&gt;- S32 Design Studio for ARM Version 2018.R1&lt;/P&gt;&lt;P&gt;However, I am facing issues during the SDK and ISELED Driver installation step (Chapter 3).&lt;/P&gt;&lt;P&gt;Problems encountered:&lt;/P&gt;&lt;P&gt;1) The update site provided in the manual:&lt;BR /&gt;&lt;A href="https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" target="_blank"&gt;https://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite&lt;/A&gt;&lt;/P&gt;&lt;P&gt;→ This link is not accessible / not responding.&lt;/P&gt;&lt;P&gt;2) Alternative attempt:&lt;BR /&gt;- Downloaded "S32 Design Studio for ARM v2018.R1 Update 9 with S32 SDK S32K1xx RTM 3.0.0"&lt;BR /&gt;- Tried installing using local archive (zip file)&lt;/P&gt;&lt;P&gt;→ Installation process hangs for a long time and eventually fails.&lt;/P&gt;&lt;P&gt;Additional notes:&lt;BR /&gt;- Clean installation environment (IDE reinstalled)&lt;BR /&gt;- Tried multiple times including reboot and fresh workspace&lt;BR /&gt;- Issue persists consistently&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1) Is the update site still valid?&lt;BR /&gt;2) Is there an alternative official installation method for ISELED SDK and driver?&lt;BR /&gt;3) Is there a recommended compatible SDK version (e.g., RTM 3.0.0 vs 3.0.3)?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;It is frustrating because the process leading up to the error on every attempt is so long.&lt;/P&gt;&lt;P&gt;I really need help to solve this problem.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Apr 2026 02:33:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ISELED-SDK-installation-issue-on-S32DS-ARM-2018-R1-Update-site/m-p/2353410#M14226</guid>
      <dc:creator>junghoolee</dc:creator>
      <dc:date>2026-04-20T02:33:26Z</dc:date>
    </item>
    <item>
      <title>Re: ISELED SDK installation issue on S32DS ARM 2018.R1 (Update site not working / Local update fails</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/ISELED-SDK-installation-issue-on-S32DS-ARM-2018-R1-Update-site/m-p/2356942#M14232</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please use S32DS for ARM v2.2 - it is compatible with Iseled v3.9.0&lt;/P&gt;</description>
      <pubDate>Tue, 28 Apr 2026 06:14:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/ISELED-SDK-installation-issue-on-S32DS-ARM-2018-R1-Update-site/m-p/2356942#M14232</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2026-04-28T06:14:16Z</dc:date>
    </item>
  </channel>
</rss>